Solutions
Waterway traffic is increasing and is having an impact on global transportation, the food chain, national defense, and even leisure time. More than 100,000 commercial and 25,000 naval vessels are operating globally. Currently 80% of all cargo passes through harbors, making them the world’s busiest hubs for bulk goods.
Look around a modern ship and you’ll find Danfoss hard at work reducing energy costs and emissions in the engine room and beyond.
On commercial and naval vessels, from cruise liners to cargo vessels to container ships, you can gain significant advantages in safety, speed, logistics, efficiency, as well as by reducing emissions to an absolute minimum. Choose from a wide array of Danfoss marine solutions for fire safety, clean water on-board, close monitoring of all engine functions, and accurate and flexible power conversion control to meet on-board and on-shore process needs.
You can gain the benefit of our extensive experience with ocean-, sea-, lake-, and river-going vessels that carry cargo or passengers, through to vessels that are built and equipped for special work at offshore sites, such as at wind farms or oil rigs.

Danfoss air conditioners are durable, energy efficient and affordable, you will find solutions for residential and commercial air conditioning applications.

Ventilation, air conditioning and indoor air quality (IAQ) are top priorities when ensuring the comfort and safety of passengers and staff - including fire safety. Danfoss VFD increase precision, save energy and extend application lifetime of the entire HVAC system.

All-wheel steering is one example of how Danfoss is at the forefront of machine versatility. This helps customers getting the most out of their equipment. Electrohydraulic steering system enables operators to manually adjust the steering mode, allowing them to best match machine performance to the task at hand.

Danfoss offers anti-stall solutions to automatically manage the power needs of the machine to prevent stalling.
Applications

It is mandatory that Danfoss AC drives are certified by the world’s leading classification authorities. See below for a brief description of the marine type approvals and to download the certificates.

Danfoss pressure sensors are ideal for accurate and reliable level measurement in overhead water storage tank systems.

Whatever your water system ambition, iC7-Aqua delivers it. The next-generation variable frequency drive for water applications improves pump efficiency, energy performance, and power quality across modern water infrastructure.

Adiabatic cooling is a highly energy efficient method of reducing air temperature by using the natural cooling effect of water evaporation. Danfoss water nozzles atomize water into ultrafine droplets, enabling rapid evaporation and effective cooling without the need for mechanical refrigeration.

Visit our Marine Competence Center
Located in Holmestrand, Norway, our Marine Competence Center provides the best possible solutions for our customers and partners. We also offer training in marine with our extensive application knowledge from the industry.
Learn more