Solutions
A secure and efficient energy supply is fundamental for the independence and environmental sustainability of any society. As cities and nations grow, their need for energy rises, requiring new and more sustainable energy sources. There are massive energy savings to earn by optimizing energy distribution and applying energy efficiency measures. At the same time, renewable sources such as wind farms and solar PV parks supplement and replace traditional fossil-fuel power plants.
Underground and deep-sea deposits contain fuel sources for the energy sector such as coal, oil, and gas, as well as minerals and metals that are valuable to the manufacturing industries of our shared planet. In each of these industries, you can use Danfoss solutions to improve sustainability and cost-effectiveness whilst reducing capital and operating expenditures.

Danfoss air conditioners are durable, energy efficient and affordable, you will find solutions for residential and commercial air conditioning applications.

Ventilation, air conditioning and indoor air quality (IAQ) are top priorities when ensuring the comfort and safety of passengers and staff - including fire safety. Danfoss VFD increase precision, save energy and extend application lifetime of the entire HVAC system.

All-wheel steering is one example of how Danfoss is at the forefront of machine versatility. This helps customers getting the most out of their equipment. Electrohydraulic steering system enables operators to manually adjust the steering mode, allowing them to best match machine performance to the task at hand.

Danfoss offers anti-stall solutions to automatically manage the power needs of the machine to prevent stalling.
Applications

It is mandatory that Danfoss AC drives are certified by the world’s leading classification authorities. See below for a brief description of the marine type approvals and to download the certificates.

Danfoss pressure sensors are ideal for accurate and reliable level measurement in overhead water storage tank systems.

Whatever your water system ambition, iC7-Aqua delivers it. The next-generation variable frequency drive for water applications improves pump efficiency, energy performance, and power quality across modern water infrastructure.

Adiabatic cooling is a highly energy efficient method of reducing air temperature by using the natural cooling effect of water evaporation. Danfoss water nozzles atomize water into ultrafine droplets, enabling rapid evaporation and effective cooling without the need for mechanical refrigeration.