• My Apps
    My Apps You will have the option to use My apps once you login.

Make sound chiller investments with ChillerROI

Wednesday, December 5, 2018

ChillerROI makes the complex decision of buying a chiller simple by comparing two chillers side-by-side. Get the information you need to make a sound financial investment that will pay off for years to come.

Starting a new construction project comes with a variety of complex decisions; one of the most important being the selection of a chiller. Choosing the right one is crucial — there are multiple factors to consider and the consequences can be far-reaching and expensive.

We're excited to announce a new tool that can help take some of the pressure off the decision and eliminate guesswork.

Introducing ChillerROI, a free mobile app that helps you compare chiller solutions and decide on the best long-term investment.

When it comes to choosing a chiller, a main consideration is return on investment, or ROI. The goal is to purchase a chiller that delivers significant energy cost savings in the long run — savings that help pay for the initial investment in the chiller itself. High-efficiency chillers can have a payback time as fast as two to three years, and then continue to deliver energy savings over their lifetime.

By using ChillerROI at the start of the chiller-selection process, you can make a wise investment with long-running benefits. You just need to enter a few key pieces of information, such as chiller efficiency data, local electrical rates, and initial cost. The app then compares the data and displays it on an easy-to-read graph that you can export and share. 

ChillerROI is available for download for free on Google Play and the iTunes Store now.

Download ChillerROI on Google Play
Download ChillerROI on the iTunes Store

Visit the ChillerROI page to learn more.