Flexible Electric Heating solutions for indoor comfort and outdoor safety
As the global supplier of electric indoor and outdoor heating solutions, we master advanced, heat-control technology that optimizes comfort, safety and energy savings.
Electric heating videos on YouTube
You can see all our videos about Electric Heating on a dedicated playlist on YouTube. Follow the link below.
Warranty
How to register for an electric heating warranty
Save time with quality & most comprehensive warranty for electric heating installation covering not only product replacement or repair but also transportation, installation and surface / floor costs
Support
Our technical support is at your service
Our technical support will help you with:
- calculations for e.g. how many and which type of cables / mats are recommended in a project.
- how to install products – what to do and what to avoid
- consulting during installation process
- open questions or issues after installation
But first check our FAQs on specific product pages (link), check our video channel (link) and review calculation tools [link to Tools and App tab]. If you don‘t find the right answers Contact us / contact us for technical support.
80 yrs of experience 80 years and product innovation
For 80 years our solutions for outdoor safety and indoor comfort have been improving people’s quality of living.
Products
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Heating Cables
Outdoor heating cables are used for efficient snow removal and ice prevention. They provide safety for people, buildings, and the environment. It is a sustainable solution for a green and clean future through low energy consumption during the frost period.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Self-limiting cables
Self-limiting heating cables are designed with a temperature-dependent resistant element between two parallel copper bus wires. When the bus wires are connected to the mains, a current goes through the temperature-dependent resistant element which will then heat.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Digital controllers
Digital controllers have unique features allowing you to reduce energy waste. Equipped with temperature and moisture sensors, control modes, and special functions, they ensure accurate temperature settings, reducing energy consumption costs by up to 40 percent.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Heating Mats
The outdoor heating mats are designed for melting ice and snow and may be installed into special mastic for ground, grass and asphalt constructions. Mats are available in different lengths for two power supply options—230 and 400 V.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Analogue Thermostats
Analogue thermostats are electronic control units allowing setting the heating system type and adjustment of control parameters.
Benefits of electric underfloor heating
A comfortable ambient temperature and quick response time are just a couple of the benefits electric heating offers. Learn more about these and other benefits of electric heating.
Applications
Case stories
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Electric heating by DEVI provides energy-efficient heating solution for near-zero energy housing complex
For decades, many have considered electricity to be an inefficient heating source, associating it with high energy bills and pollution. However, times are changing. Now, the combination of electric floor heating and solar panels are an energy-efficient option for homeowners. Yes, the future is indeed electric, as this case from Koblenz, Germany shows.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }The Bjørvika Tunnel, Oslo, Norway
Electric heating for the immersed tunnel in Norway.
The Bjørvika Tunnel is a motorway immersed on European Route E18 in the city center of Oslo. The tunnel links Festning tunnel in Oslo west with Ekeberg tunnel in Oslo east. The completed tunnel has an unbroken length of six kilometers. The Bjørvika Tunnel is the first immersed tunnel in Norway.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Electric heating system to prevent the condensation in the Woolworths Distribution Centre
The Woolworths Distribution Centre was experiencing condensation due to the temperature differences between the cold storage facility and their offices. This resulted in water dripping hazards in the meeting rooms, canteen, and offices.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Pipe tracing in 600 Suzhou apartments China
Suzhou city was founded in 500 BC. is nowadays a major city located in the south-eastern Jiangsu Province of East China, about 100 km (62 mi) northwest of Shanghai. It is a big economic center and local point of trade and commerce, and the second largest city in the province, after its capital Nanjing.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Electric heating systems for the conservation of old castles
The Örebro Castle is a medieval castle fortification situated in the scenic region of Närke, Sweden. The castle lies on an island by the river Svartån. The oldest part of the castle, a defense tower, was erected in the latter half of the 13th century, but its present appearance, the Örebro Castle, was constructed over the last century. Since 1935, the castle has been a national Swedish monument.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Supporting constant temperature at Montague Apple Orchard and Warehouse in Victoria Australia
Montague Apple Orchard, established in 1948, is a key player in the Australian food manufacturing industry with a 70-year legacy.
In their upcoming Narre Warren Cold Storage Warehouse, a constant temperature of 1°C is required to avoid condensation.
Learning
Visit our Learning Center
Danfoss offers online training materials for technicians and designers working with electric heating. There are 14 e-lessons available free and on-demand through Danfoss Learning portal. For more information, register in our support section by following the link or find the overview of available relevant trainings in the table below.
News
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Did you know? 90% of DEVI product portfolio has Environmental Product DeclarationWednesday, April 17, 2024
EPD (Environmental Product Declaration) is a report detailing the environmental footprint associated with a product.
With EPD, DEVI brand ensures and comprehensively demonstrates the environmental impact of our products at various stages of their life cycle.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Efficient de-icing solution for safer outdoor areasWednesday, January 25, 2023
Frost and snow protection of outdoor areas
Address seasonal changes with energy-efficient systems, using electric heating mats or cables to commercial and residential areas against snow, ice and frost damage. -
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Switching to electric heating as a primary or comfort heating source is a future-proof decisionFriday, November 18, 2022
With energy costs – including the cost of electricity – rising in most European countries, the last thing on peoples’ minds might be switching to electric heating as a primary or comfort heating source for their homes. But could it be that electric has much more potential than people think?
Articles
DOs and DON’Ts for Indoor Electric Heating
Electric Heating is an energy-efficient and environmentally friendly floor heating solution. You can use it for either newly constructed or renovated homes.
Contact us
For further information, please contact us for technical support