For safe and efficient data center cooling
Cooling of IT equipment in data centres is an increasing challenge for operators and design engineers. Power management is the major challenge, with energy consumption and heat loads increasing in step with the server density. Meeting these challenges is essential for ensuring the safety and availability of the data.
Data center cooling technology:
Other important factors in data center cooling solutions are:
- Cost optimization: cooling can be up to 50% of the overall energy cost in a data center
- Precise humidity control and better control of static electricity
- Minimum start-up current for situations where the power grid is sensitive to load, reduced downtime, and increased lifetime of the overall system
Why choose our variable speed compressors for process cooling?
The first major benefit is the overall energy saving.
Other benefits include:
- Flexibility with combined compressor and free cooling
- Quick and smooth adaptation to varying loads; Danfoss inverter technology modulates cooling between 25 and 100%, saving substantial amounts of energy, especially in part-load operation. Experience shows that savings of up to 50% can be achieved in energy consumption. This significantly reduces the PUE values (ratio of power supplied to the data center divided by power consumed by the IT infrastructure) (see Figure 1).
Figure 1: Potential energy saving in a packaged unit equipped with a single inverter compressor compared with a unit equipped with a fixed-speed compressor.
- Actual energy efficiency improvements will vary depending on the data center design and the configuration of the cooling systems. However, recent experience has shown that installing a VSH variable speed compressor solution into a unit previously using traditional On-Off compressors can reduce the annual energy consumption of the cooling unit by as much as 50%. Danfoss inverter scroll compressors are the most energy-efficient solutions available on the market today.
- Stable and precise temperature control, with very consistent and stepless adaptation to required cooling load. Whatever the variation in ambient temperature or outside temperature, the system can maintain a set point temperature to within ±0.2°C thanks to the capacity modulation system (see below figures).
- Reduced noise under partial load conditions facilitates the integration of the unit in the surrounding.
- Reduced start-up current is an additional benefit with variable speed technologies, since the compressor rarely needs to start at full load, and since the Danfoss inverter has a very soft start with very low in-rush current. This benefit solves the problems that arise in areas where electric power is unstable, avoiding a peak in demand.
Products
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Inverter scrolls - VZH
Danfoss inverter scroll compressor VZH offers effectiveness and reliability. Over 30% energy savings is possible in rooftops, chillers, close controls etc.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Turbocor® - TTS
Danfoss Turbocor®model TTS oil free compressors are available in four different models ranging from 60 tons to 200 tons / 200 to 700 kW utilizing R134a or low GWP R513A.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Turbocor® - TGS
Danfoss Turbocor model TGS oil free compressors are available in 5 different models ranging from 40 tons to 150 / 140 kW to 540 kW utilizing ultra-low GWP R1234ze or R515B.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Inverter scrolls - VRJ
Danfoss inverter scroll compressor solutions for commercial air conditioning and process-cooling applications. R410A, single units. VSH: first-generation commercial inverter scroll compressors with frequency converter CDS302. VZH: second-generation commercial inverter scroll compressors with frequency converter CDS303. VRJ: first high-tier residential inverter scroll compressors with frequency converter CDS801.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Inverter scrolls - VSH
Danfoss inverter scroll compressor solutions for commercial air conditioning and process-cooling applications. R410A, single units. VSH: first-generation commercial inverter scroll compressors with frequency converter CDS302. VZH: second-generation commercial inverter scroll compressors with frequency converter CDS303. VRJ: first high-tier residential inverter scroll compressors with frequency converter CDS801.
Case stories
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Denmark's new climate-friendly hospitality giant depends on Turbocor® oil-free chiller
The new Alsik hotel in Southern Denmark sets a higher standard in energy-efficiency and is built to reach 76% CO₂-neutrality. A main contributor is the 900-kW chillers by Clint (a company of G.I. Industrial Holding) which features award-winning Danfoss Turbocor oil-free compressors.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Oil-free compressors maintain consistent performance over time
Danfoss conducted a study to see how long term operation affected performance on Danfoss Turbocor® compressors. The results showed that oil-free, magnetic bearing compressors maintained consistent performance even after 10+ years of operation.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Wind power
Wind turbine producing water cooled by an energy efficient refrigeration system featuring inverter scroll compressor
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Satellite launch towers
The satellite launch tower is a vital facility. Reliable energy efficient inverter HVAC unit in this critical application was secured with Danfoss solution.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Research laboratories
Renovation of Key Laboratory in Shanghai illustrates the benefits of temperature control and energy savings in critical applications with inverter technologies
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Process chillers
Variable speed with Danfoss Turbocor Oil free centrifugal compressor guarantees reliable process cooling and efficient comfort cooling in factory
Contact us
For further information, please contact us.