![Hybrid ferries connect the city of Amsterdam nonstop](/media/2340/marine_cs2_hybrid-ferries.jpg?anchor=center&mode=crop&width=520)
On Amsterdam’s IJ River, hybrid ferries powered by VACON® drives enjoy 24/7 uptime, smaller generator size, improved air quality, less noise and easy maneuverability.
GVB has a policy of reducing the emissions and environmental impact from its ferries, trams, buses and cars to an absolute minimum. So when GVB ordered 2 new ferries from Holland Shipyard they decided to use battery hybrid technology to improve fuel efficiency and reduce pollution.
Peak shaving reduces generator size
The ferries operate 24 hours 365 days per year. It takes about 4 minutes to cross the IJ River and the ferries are docked for only about 2 minutes before departing on the next trip.
A 100% battery-powered electric ferry was not possible as the time spent docked in port was too short to charge the batteries from a shore power connection. Instead, GVB decided to use electric propulsion with diesel- powered generators and Lithium-Ion batteries to shave the power peaks.
This allowed them to downsize the generators, as these batteries enable the generators to run very efficiently with an almost constant load.
Hybrid improves air quality …
To reduce the remaining air pollution the diesel engines are fitted with efficient exhaust gas cleaning systems, also known as SCR (selective catalytic reactor), which remove toxic gases and particles.
The IJ Ferries 60 and 61 already fulfil the new stricter air pollution rules, which will apply from 2019/2020. This contributes to improving the air quality and reduces noise for the citizens of Amsterdam and for the millions of tourists using the ferries.
… and maneuverability
The skippers are very happy with the new ferries: The ferries are just as easy to handle as the conventional diesel-powered sister ships, but they are much quieter. The low noise level makes the ride a pleasure for both passengers and crew.
24/7 uptime
The city of Amsterdam considers the ferries to be “floating bridges” – which help to tie the northern and southern parts of Amsterdam ferries. The floating bridges are free of charge for the passengers.The two redundant DC grid systems were chosen for safety reasons – but the short circuit protection was a challenge. GVB is satisfied with the solution and will consider the same hybrid ships the next time there is a need for new ferries.
All power conversion installations
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Aurora Botnia: Världens första färja som drivs med iC7-MarineFINLAND: Bil- och passagerarfärjan Aurora Botnia är utrustad med ett hybridelektriskt framdrivningssystem som drivs av vätskekylda iC7-frekvensomriktare från Danfoss.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Avkarbonisering av nästa generations utbildningsfartyg, SkulebasNORGE: Det nya utbildningsfartyget på fiskeriskolan i Måløy använder mindre diesel och släpper ut mindre CO2, samtidigt som det uppfyller fiskeindustrins stränga krav.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Adjö till NOx-partiklarGrovfjord Mekaniske Verksted i Norge has utformat en av världens första helt eldrivna arbetsbåtar. Inget motorbuller, inga dieselångor och noll utsläpp. Detta är elektrifiering till havs, och frekvensomriktare från Danfoss har bidragit till att förverkliga det.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Elektrisk arbetsbåt säger adjö till NOx - utsläppDetta är en av världens första helt elektriska arbetsbåtar – konstruerad och byggd av Grovfjord Mekaniske Verksted i Norge. Den har ingen bullrig motor, avger inga dieselångor, ger noll utsläpp och är extremt lättstyrd. Detta är elektrifiering till havs – och frekvensomriktare från Danfoss har bidragit till att förverkliga det.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Hybrid powertrain improves tugboat economy and maneuverabilityThe Telstar saves 20% on operating costs compared to traditional tugboats.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VACON® drives power hybrid ferries 24/7Passenger ferries bridge Amsterdam’s IJ River, keeping the city connected around the clock. Hybrid propulsion powered by VACON® drives ensures 24/7 uptime, smaller generator size, better air quality, less noise and easy maneuverability of the vessels.