Danfoss VLT drives are used to control the pumps in the Randers Rainforest tropical zoo in Denmark. The VLT HVAC Drives are used to control the pumps in the water cleaning processes. They not only reduce the energy consumption but also free up a whole year's manpower to manually control the valves in these processes. The IP 55 cabinets of the drives and the coated circuit boards that comply with the 3C3 protection standard are perfect for the installation environment where air humidity often reaches 100%.
Danfoss VLT® drives used in Randers Rainforest
onsdag 15 januari 2014