EKE 1 A,B,C and D
The reason could be that EKE 1A,B,C and D controllers has reset its settings after 32000 hours of operation and a consequent power cut off. This can be corrected by the below methods.
If the software version is 2.04, use the patch provided to permanently patch the product.
Check product label for identification of software version. Below is an example of where to find the information on the product label.
- Link to download Patch for EKE 2.04
- This video will assist you on how to do the patch.
- If the software version is 2.02 or lower, check the video and instructions to reset and reconfigure the product.

If the software version is 2.04, use the patch provided to permanently patch the product.
Below video will assist you on how to do the patch.
This SW version already includes the patch. No action needed from your side.
No, these versions only have temporary solution of reset and reconfigure the product. The patch should not be used in this case.
Check the below video and instructions to reset and reconfigure the product.
EKE 1P controllers
The reason could be that the EKE 1P controller has reset its settings after 32.000 hours of operation and a consequent power cut off.
It can happen with EKE 1P controller software (SW) 2.14 or older and if the controller is used with Application 2 as standalone driver (for example as valve driver with AK-CC55) or with Application 1 as extension module for AK-PC 572 but with User Defined valve. In both cases the recommendation is to update the controller to SW 2.15 or newer.
If EKE 1P is used as extension module for AK-PC 572 with a standard Danfoss valve, no further action is needed.
Here you can find step-by-step instructions on how to update the EKE 1P software.
Here you can find SW version 2.15 for updating.

No. After the update, the settings will be reset to default values, so make sure you note down the controller settings before updating.
By reading the settings on the remote display.
No. SW for the EKE 1P cannot be used with EKE 1A/B/C/D as well as EKE 1A/B/C/D SW cannot be used with the EKE 1P.