NETHERLANDS: Air at the port of Scheveningen is cleaner than ever thanks to a new shore supply facility. Thanks to the shore power supply, berthed vessels can shut down their diesel generators and instead buy sustainable power using an app.
The alternative electricity supply eliminates air pollution and reduces noise and vibrations when ship engines are idle. It’s so convenient and popular that on average, the harbor saves 1,000 liters marine diesel daily, resulting in dramatic reductions in air pollution from particulate matter, nitrogen oxides (NOx) and sulphur oxides (SOx) in addition to substantial CO₂ savings.
“The system has been successfully working for two years now, and we’ve had no problems at all with any of the Danfoss components: They’re totally reliable”, explains Maarten Hektor, Managing Director, Involtum
100% renewable energy
The installation of shore power in Scheveningen harbor is a major part of The Hague’s Air Quality Action Plan, which outlines what the municipality is doing together with businesses, residents, interest groups and the Dutch State to further improve the air quality in the city. Of course, only 100% Dutch sustainable wind energy is used in the installation.
Power connection for many vessel types
While shore power in the Second Harbor already existed for cutters, small fishing boats and pleasure vessels, this major new industrial-scale installation in the other two harbors extended capacity to many more vessels.
The new shore supply system serving the First and Third Harbors is a first for the Netherlands in terms of its large scale, its technology, and its convenience for users. The system was built using a Danfoss VACON® NXC series low harmonic drive to convert grid power to adapt the frequency to the ship’s grids. The system has eight power outlets each with a communication system allowing the ship’s engineer to connect and pay for power using an app.
Explore more
Discover how shore supply helps ports meet emission targets
All power conversion installations
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }PSW and Danfoss: Flexible onshore power for berthed cruise ships
NORWAY & SWEDEN: PSW (Power and Automation AS) paired up with Danfoss to create compact OPS solutions in three Nordic harbors: Stockholm, Ålesund and Haugesund/Karmsund.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }World’s first ferry powered by iC7-Marine: Aurora Botnia
FINLAND: The Aurora Botnia cargo and passenger ferry is equipped with a hybrid-electric propulsion system, powered by liquid-cooled iC7 drives from Danfoss.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }VACON® drives electrify passenger ferries in Oslo Fjord
NORWAY: Electrification of the Nesodden ferries has reduced CO2 emission in the port of Oslo. VACON® drives and power converters play a key role onboard.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Decarbonizing the next-generation training ship, Skulebas
NORWAY: The new training vessel at Maløy Fishing School uses less diesel and emits less CO2, while also meeting the rigorous demands of the fishing industry.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Where smart ferry charging begins with a smart grid
NORWAY: The Hareid-Sulesund ferry operations have reduced CO2 emissions by 7000 tonnes annually with the introduction of electric vessels. In transitioning ferries from diesel to pure electric power, powerful onshore support is essential, in the form of reliable infrastructure for rapid charging capacity and stable grid supply. The systems on board and on shore act as a single system – a sophisticated and competitive system developed by Norwegian Electric Systems (NES) using Danfoss technology.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Royal IHC Scheldt River pioneers new environmental standards in dredging with flexible MV drives
A Danfoss medium-voltage drive solution boosts an inboard dredge pump and increases energy efficiency with a small footprint, minimum weight and low volume - while being robust enough to withstand the harsh marine environment.