SPAIN: Through innovation and planning, Volkswagen aims to continuously reduce energy consumption and the associated CO2 emissions at its factory sites. One good example is in air conditioning. The demands placed on the air conditioning of buildings increase steadily. Axial fans can make a significant contribution to combining technical requirements with sustainable building design.
Therefore in 2018, two production sites in two separate countries installed air handling units with new technology and highly efficient axial fans controlled by VLT® HVAC Drive FC 102: Porsche in Stuttgart/Zuffenhausen, Germany and Volkswagen Navarra in Pamplona, Spain. The upgrade at Volkswagen Navarra resulted in impressive 20% energy savings in AHU operation.

Discover how Volkswagen achieved 20% energy savings in AHU operation
The new trend-setting AHU technology installed at Volkswagen fully met all expectations of Asier Matorell, Factory Planning Manager, Volkswagen Navarra (left) and Axel Rossmannek, Head of Supply Planning, Volkswagen Wolfsburg.

Pioneering sustainable ventilation technology
The ventilation had to be completely renewed for one of the largest production buildings at the factory. Higher air volumes were needed and the space available for the installation of the equipment was insufficient. Therefore, a new installation location for the AHUs had to be found on the roof. The large 80,000 m³/h units were placed on a steel platform on the connection between two buildings. In addition to saving energy, the criteria unit size, weight saving and noise reduction were therefore also key requirements.

Intelligent interaction
The high demands could only be met with the new generation of air handling units, optimally utilizing the highly efficient axial fans from NOVENCO, with VLT® HVAC Drive FC 102. Performance exceeded all expectations. The ZerAx® axial fans currently represent the world’s leading fan technology with fan efficiencies of up to 92%. NOVENCO, however, went one step further by optimizing the ZerAx® even more for use in the air handling units. Here the Danfoss EC+ Concept was an essential contributor to the energy savings.
The key phrase here is intelligent interaction of the system components. This interaction is embodied in the term EC+ and is developed in cooperation between Danfoss and NOVENCO. Only the optimal interaction of the system components fan - motor - electronics – diffuser, makes the full potential of a highly efficient fan realizable.

What is the Danfoss EC+ Concept?
When building an HVAC system, to get the highest performance and system efficiency, the individual components – motor, drive and fan – need to be flexible and broadly compatible with each other. For instance, if you specify a high-efficiency motor that is only compatible with lower efficiency fans, the overall system efficiency would suffer and would not reflect the high performance – and investment – in the individual components.
Danfoss Drives’ EC+ concept allows ventilation system designers to combine a VLT® HVAC Drive with the most efficient fan and permanent magnet motor.
Advantages of the EC+ concept:
- Free choice of motor technology: PM, asynchronous or synchronous reluctance with the same AC drive
- Device installation and operation remain unchanged
- Manufacturer independence in the choice of all components
- Superior system efficiency thanks to a combination of individual components with optimum efficiency
- Retrofitting of existing systems is possible
- Wide range of rated powers for standard, PM and synchronous reluctance motors

Get even more drive in your HVAC
Products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }DrivePro® ServicesEvery AC drive application is different. DrivePro® Services is a collection of tailor-made products designed around your needs.
From optimized spare part packages to condition-monitoring solutions, customize our products to support your business through the different lifecycle stages of your AC drive.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VACON® 100 FLOWDedicated functionality that improves flow control and saves energy in industrial pump and fan applications.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® HVAC Drive FC 102This tough and savvy FC102 drive enhances pump and fan applications in building management systems, and runs outdoors in most climates.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® Refrigeration Drive FC 103FC 103 is dedicated to controlling compressors, pumps and fans for significant energy savings in refrigeration plants.
Read more about Danfoss HVAC solutions
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Condition monitoring of HVAC/R systemsIn air flow and indoor air quality-related applications, condition monitoring functionality improves system uptime and competitiveness by preventing issues before they occur.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Drives for fansGet more out of your air handling units, using fan control that gives you easy air filter monitoring and built-in fire safety features.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Drives for fans in commercial buildingsWith user-friendly interfaces, distributed intelligence and reduced power consumption, Danfoss AC drives optimize the performance of fans.
More AHU case studies
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Ventilation is more energy-efficient in this Illinois factoryUSA: The Danfoss Loves Park factory upgraded existing ventilation with the Danfoss Novenco EC+ concept, achieving a 59.8% reduction in emissions compared to the previous system.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Wind tunnel achieves 99.5% uptime with Danfoss DrivePro®Belgium: Thanks to Danfoss DrivePro® services, LuxFly has achieved 99,5% uptime in Europe’s largest vertical wind tunnel that is used for skydiving.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }How did this smart factory reach carbon-neutral?POLAND: The new Danfoss production hall in Grodzisk Mazowiecki has reached carbon-neutrality, thanks to full electrification, energy-saving solutions such as Danfoss drives, and energy from renewable sources.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Retrofitting Keppel Bay Tower for a Zero Energy futureSINGAPORE: With Danfoss EC+ concept for HVAC systems, Keppel Bay Tower uses 45% less energy and has achieved Green Mark Platinum Zero Energy building status.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Drives secure fresh air inside South America’s tallest buildingA huge number of Danfoss drives secure comfortable temperatures and cut down energy use inside Chile’s famous Costanera Center.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Driving maximum uptime in aseptic pharmaceutical productionDENMARK: A leading global pharmaceutical company was determined to find an intelligent HVAC solution to prevent downtime with real-time system monitoring and customizable instant alarms. Plus, the solution needed to fit within the organization’s ambitious digitalization strategy. The solution: Danfoss VLT® HVAC Drive FC 102 with integrated condition-based monitoring.