Increased focus on the environmental impact from the marine industry has led to strict regulations on ballast water treatment. This means that vessel owners have to implement Ballast Water Treatment Systems (BWTS) to ensure compliance with applicable legislation.
This article explores the challenge of ballast water and the solutions required to comply with the regulation.
The challenge of ballast water
The problem of invasive species carried in vessels’ ballast water is largely caused by the ever-growing trade and traffic across the oceans. The huge amounts of ballast water pose serious ecological, health and economic challenges, as it carries invasive species – bacteria, microbes, plankton, eggs, cysts and larvae - from one part of the world to another.
Facts about ballast water and invasive species
- It is estimated that around 6-10 billion tons of ballast water are moved around the world in ballast tanks every year.
- Every day, an estimated 7,000 marine and coastal species travel unnoticed across the world’s oceans, silently stowed away in vessels’ ballast water tanks.
The effect of the unwanted species has been devastating to local eco-systems. Data shows that the rate of bio-invasions continues to grow at an alarming rate, and new areas are being invaded all the time.
Since the volumes of seaborne trade are expected to continue growing, the problem associated with ballast water may not have reached its peak yet. In order to mitigate the problem, the IMO Ballast Water Management legislation came into force in September 2017.
Related products
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }EV212B Solenoid valves with FKM isolating diaphragm 2/2-way direct-operated
The compact 2/2-way solenoid valve EV212B with an isolating diaphragm design ensures no fluid can enter the armature area meaning the valve can be used for aggressive fluids.