After several rounds of testing and qualification, Climaveneta has chosen Danfoss as its preferred supplier of key components for its free cooling units.
"Danfoss is one of the leading suppliers in the air-conditioning industry, offering a complete range of components that includes compressors, valves, heat exchangers, and controllers," comments Mr. Guo Minghui, Purchasing Director at Climaveneta. "Danfoss provides us not only with high-quality, reliable products, but also professional technical support that meets our challenging demands. The strong support provided by Danfoss is a major factor in our choice of Danfoss as our preferred supplier."
"Danfoss provides electric expansion valve ETS, solenoid valve EVR, and check valve NRV, among other components, for Climaveneta's air-cooled screw chiller with free cooling technology," comments Application Expert Mr. Zhou Dazhi from Danfoss: "The Danfoss ETS valve design uses a bipolar drive providing very precise flow regulation. The EVR solenoid valve is suitable for a wide range of refrigeration capacities. This allows smooth operation across a wide temperature range, as well as eliminating leaks. It is a more reliable and more efficient solution."
Mr. Zhou particularly emphasizes that: "though the NRV check valve is small in appearance, it offers both low leak risk and low noise levels. The valve ensures the correct flow direction, and the Teflon tightening ring seals perfectly with minimal closing force. This improves the efficiency and reliability of the air-conditioning system, with performance that exceeds the industry standard."
Danfoss is the market leader in the air-conditioning industry, providing a wide range of compressors, valves, heat exchangers and controllers.
Marketing Manager Ms. Zhou Qian from Climaveneta points out that: "employing free cooling technology with air-cooled screw chillers in China will enable data centers and the cloud computing sectors to perform outstandingly."
"Both Climaveneta and Danfoss are well-known European companies in the refrigeration and air-conditioning industry," concludes Lu Liuliu, Regional Sales Manager of Danfoss China. "Climaveneta Chat Union Refrigeration Equipment (Shanghai) CO., LTD is a joint venture of Climaveneta S.p.A. and Chat Union Group HK. Danfoss has established a close relationship with Climaveneta, steadily growing the two companies' business cooperation through high-quality products and services, fostering a true win-win situation."