Efficient and reliable Danfoss components provide fresh water aboard the cruise ship, Icon of the Seas
WatMan Engineering chose Danfoss high-pressure pumps and energy recovery devices as key components in the SWRO plant that supplies fresh water to the world’s largest cruise ship, Icon of the Seas. The Finnish water treatment specialist will also rely on Danfoss to keep the water flowing on the next two ships in the Icon class.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }High-pressure pumps for SWRO applicationsThe range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }iSave® energy recovery devices for high-pressure membrane applicationsWith a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day