The domain Louis Moreau in Chablis is a 50-hectare family estate. Today it is owned by Louis Moreau, representing the sixth generation of his family’s vine growers. With 80% of production being exported, the vines of Chablis are well known in France and worldwide.
Since 2015, late spring frost at night started happening in Chablis causing big challenges for the Chardonnay vines. On average they lasted yearly for 5 nights.
Since that time Louis Moreau enterprise has used candles to protect vines against frost. But this solution was expensive from the perspective of time, energy, and human efforts.