Pressure independent control valves work miracles in Swedish housing estate

Wednesday, April 22, 2020

Winters are long, dark and freezing in Gothenburg in Sweden. A nice, warm living room and plenty of hot water in the shower are therefore essentials to get through the cold season. Unfortunately, the people living in the apartments of the Göteborgshus housing estate had neither. The supply of heating and hot water was unstable, and complaints piled up in the office of the facility manager. Moreover, the district heating return temperature was much too high, which resulted in substantial penalty fees and high energy bills from the local district heating company.

First step: Installation of Energy Management System

Energy control experts from Dunderon were called in to help solve the problem. After close inspection of the existing heating and hot water installation, they introduced the Dunderon Energy Management System and mounted electronic controllers on the decentralized substations for room heating and the central substation for domestic hot water.
After that, things started to improve in the apartments. The room temperatures were comfortable, and the supply of hot water was more stable now. However, the district heating utility was far from satisfied. The flow on the primary district heating side was even higher now, and they saw no improvement on the return temperature. The energy bill was rising, and the housing association and residents had to pay dearly to keep warm. Obviously, something was wrong on the secondary side, and Dunderon asked Danfoss to help provide a solution that would solve the problem once and for all.

Second step: PICVs and new heat exchangers solve the problem

In close collaboration, the partners decided to replace the existing heat exchangers of the substations with new micro-channel heat exchangers from Danfoss. Furthermore, the existing two-way control valves were replaced by AVQM pressure independent control valves for district energy systems.
The new system design allowed some fundamental changes to the basic operating parameters in the secondary loop. The pump flow level could be lowered from 40 % to 20 %, and the supply temperature was reduced by ten degrees to only 60°C.
The result fulfilled everybody’s expectations. Residents now enjoyed a comfortable indoor environment and hot water at all times, while the housing association could cut the energy costs by as much as 25 %. They even received a bonus from the district energy company in return for low flows and low return temperature.

Benefits of substation upgrade with pressure independent control valves and new heat exchangers

How AVQMs solve the problem

The pressure independent control valves:
• Prevent oscillation over control valves
• Increase precision of temperature control
• Enable reduction of supply temperature – no overflow
• Lower return temperature to district heating system

Related products

  • if (isSmallPicture) { Differential pressure controllers- Danfoss; } else if (isBigColumns) { Differential pressure controllers- Danfoss } else { Differential pressure controllers- Danfoss }
    Differential pressure controllers

    Differential pressure controllers keep a constant and lower differential pressure across a motorized control valve or a total system/substation. This eliminates pressure variations and improves temperature control quality.

  • if (isSmallPicture) { Differential pressure, flow and temperature controllers- Danfoss; } else if (isBigColumns) { Differential pressure, flow and temperature controllers- Danfoss } else { Differential pressure, flow and temperature controllers- Danfoss }
    Differential pressure, flow and temperature controllers

    Balance your network, save energy and improve end-user comfort by hydronic balancing and control of district energy networks. Optimal hydronic balance and perfect temperature control are the key to maximizing the efficiency of heating or cooling networks.

  • if (isSmallPicture) { Virtus | Heavy-duty Pressure and Flow Controllers; } else if (isBigColumns) { Virtus | Heavy-duty Pressure and Flow Controllers } else { Virtus | Heavy-duty Pressure and Flow Controllers }
    Virtus | Heavy-duty Pressure and Flow Controllers

    A new generation of Virtus intelligent ready pressure and flow controllers are here to ensure high durability, improved functionality and performance in district energy networks balancing. In addition, unique intelligent optimization functions iNET and iSET will save even more energy.