• My Apps
    My Apps You will have the option to use My apps once you login.

Energy comfort in Prime Tower, Zurich, Switzerland

Wednesday, February 3, 2016

The Prime Tower in Zurich is a building of many records. With its 126 meters it is the tallest building in Switzerland with 36 floors and 40,000 square meters accommodating mostly offices. And with its more than 6,000 AB-QM valves it is also one of the biggest heating and cooling installations ever designed and installed by Danfoss.

It is one of the biggest Danfoss hydronic balancing solutions ever with more than 6,000 AB-QM pressure independent balancing and control valves to achieve the optimum balance in the heating and cooling of the tower. The advanced system ensures a stable temperature and pleasant indoor environment for the thousands of people working in the building every day.

The Prime Tower sets new standards for eco-efficiency

The Prime Tower has been designed and constructed to set new standards in Switzerland in terms of eco-efficiency. The building has been certified according to the “greenproperty” seal, a new Swiss sustainability rating measuring real estate and buildings according to five criteria: energy, materials, usage, infrastructure and life cycle. Furthermore, Prime Tower has been certified according to the international LEED Gold standard.

Swiss Prime, the owner of the building, is keen to show the way for environmental responsibility and to meet future tenants’ requirements to sustainability. Just like the hydronic balancing specialists at Danfoss, who strive to offer complete solutions that are not only cost efficient but also outstanding when it comes to energy efficiency.

Highly efficient solution

The distinctive octagon-shaped building is the winning project of a high-class competition involving top-ranking architects. The heating and cooling solution has been designed by Danfoss in close cooperation with the project’s leading designers and engineers. It is a highly energy efficient solution with a 4-pipe system (change-over) with radiant cooling and heating ceilings, 268 manifolds for the pipes and 0-10 volts thermal actuators.

Recently Danfoss supplied a similar solution to Kommerzbank in Frankfurt.

''Swiss Prime Tower represents not only an impressive piece of architecture seen from the outside, but also a unique climate and people friendly solution on the inside. The heating and cooling solution ensures high energy efficiency combined with a pleasant indoor climate for the thousands of people working in the building every day.'' Swiss sales team

About Prime Tower

  • 40,000 square meter, mostly used for office space. At ground floor cafés, shops, etc.
    36 floors, 126 meter high, making it the tallest building in Switzerland
  • AB-QM DN 15-150 with AME actuators
  • MSV-F2 DN 20-300
  • Environmental labels: LEED Gold, international standard for energy and environmental design; Minergie, Swiss standard for environmental design; Green Property, Swiss seal of approval for sustainable real estate
  • Investor/owner: Swiss Prime
  • Architect: Gigon/Guyer, Zürich

Advantages of the heating/cooling solution

  • Simple design
  • High balancing efficiency
  • Safe operation
  • Low operating costs due to hydraulic efficiency
  • Low maintenance costs
  • High energy efficiency

Related products

  • if (isSmallPicture) { AB-QM- Danfoss; } else if (isBigColumns) { AB-QM- Danfoss } else { AB-QM- Danfoss }
    AB-QM Pressure Independent Control Valves (PICV) DN15 - DN250

    AB-QM Pressure Independent balancing and Control Valves (PICV) provide both a control functionality and dynamic balancing solution for HVAC heating and cooling systems. PICVs are designed for various types of terminal units, Air Handling Units (AHU), chillers and provide high indoor comfort and energy efficiency in public and commercial buildings.