The challenge:
How to prevent condensation between storage and office rooms
The Woolworths Distribution Centre was experiencing condensation due to the temperature differences between the cold storage facility and their offices. This resulted in water dripping hazards in the meeting rooms, canteen, and offices.
The solution:
To prevent and protect against these hazards, our partner in Australia Heat Zone Distribution supplied electric heating cables to the Woolworths facilities and NWR Electrical Services performed the installation.
The result:
The 700.71m² space was segmented into 4 zones and the thermostats were integrated into switchboards for a set and forget system. This prevents condensation and allows Woolworths to compensate for the temperature differences between the cold storage and office facilities. The 2743.21 W electric heating system is an effective and easy-to-use solution to save space and lower initial costs.
Project Overview:
Application type: Indoor Heating
Area Size: 700.71m²
Installed power: 2743.21 W
Products: DEVIsnow 30T, DEVIbasic Drum Goods, DEVIreg 330, DEVIbasic 10S
Year of implementation: September 2021