• My Apps
    My Apps You will have the option to use My apps once you login.

Case Asokodit

Sunday, June 18, 2017

Asuntosäätiö Asokodit is one of the largest housing owners in Finland, owning close to 17,000 homes in 31 localities in Finland. Asokodit adopted the Leanheat concept in 2016. Initially, the system was piloted in eight housing estates in Espoo and Vantaa. In 2017, Asokodit is going to introduce Leanheat in at least 15 additional housing estates, extending the system to 1,040 flats.

Teemu Jalomäki

For a long time, heating systems in buildings have relied on traditional temperature charts based on the outside temperature only. This often leads to many problems, such as over-heating. After hearing positive experiences with Leanheat from our colleagues, we decided to explore its suitability.

Teemu Jalomäki, Real Estate Manager

Asuntosäätiö Asokodit has had good results from the first heating season.

  • Controlling the district heating system with real-time measurements and AI has reduced the peak demand of district heating by 21% on average.
  • At the same time, energy consumption has decreased, and consequently the investments in Leanheat will pay for themselves in a few years.
  • Teemu Jalomäki stresses, however, that ultimately the localisation of measurement data and AI is a much more complex matter, not just about reducing the consumption of energy.

For example, with continuous measurement in every flat, we can now carry out the balancing/fine tuning of estates with less effort and at a reduced cost.

Previously, we did use conventional heating characteristic curves and adjusted the heating separately for each building with technical maintenance. Nevertheless, temperature differences between flats could still be significant. With flat-specific temperature measurements and fine control, we could take care of the temperature imbalances.

The system also recognizes potential risks, such as unusual humidity conditions that can be extremely expensive to fix afterwards.

In the future, we are going to selectively expand the use of Leanheat in our real estate”

Leanheat® — For true energy optimization. From people to production.

Buildings account for a staggering 40 percent of the world’s energy consumption. And in Europe alone, almost a third of residential heating comes from fossil fuels.
Leanheat empowers district energy networks to optimize the operational efficiency of buildings and increase the comfort of end-users through end-to-end software solutions.