Tailored for HVAC, flexible, modular and adaptable applications, the frequency control has played a key role in the ventilation system. It was the perfect fit, both in terms of EMC requirements, safety, harmonics, long cable lengths and dimensions, as well as its ability to function in temperatures of up to 50°C without loss of power.