To protect the pristine environment during tours, the Krka National Park commissioned two hybrid e-vessels designed for a capacity of 50 passengers each. The vessels are equipped with both solar PV panels and battery storage. When the sun shines, solar cells supply power to the propulsion. When the sun disappears, the propulsion runs on battery power. In this way the e-vessels run reliably emission-free, no matter what the weather.

Silent and emission-free e-vessel
The fully-electric vessels operate a cycle of 8 hours on battery power and 12 hours on solar panels. Service speed is 5 knots, and maximum speed is 9 knots.

Optimal power conversion from solar cells to battery
The technical challenge for this e-vessel was to achieve proper functioning between the solar PV panels and battery in the driveline system. Danfoss was able to design and deliver the ideal solution thanks to its understanding of the needs of the e-vessel, and capability in handling advanced technology.

MPPT software upgrade in system integrator workshop
Danfoss cooperated with the system integrator Inmel, by providing all the necessary hardware and software for the green hybrid solution.
For the first time ever, the MPPT software upgrade was uploaded to DC/DC software on site at the system integrator workshop, and successfully tested. Danfoss provided a maximum power point tracker (MPPT) which was implemented in the DC/DC software. This enabled higher voltage on the solar panel using only the highest voltage point, resulting in more energy on the common DC bus.

Discover VACON® NXP DC/DC Converter
Related case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Where smart ferry charging begins with a smart gridNORWAY: The Hareid-Sulesund ferry operations have reduced CO2 emissions by 7000 tonnes annually with the introduction of electric vessels. In transitioning ferries from diesel to pure electric power, powerful onshore support is essential, in the form of reliable infrastructure for rapid charging capacity and stable grid supply. The systems on board and on shore act as a single system – a sophisticated and competitive system developed by Norwegian Electric Systems (NES) using Danfoss technology.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Fuel cells for electric transportation of the futureITALY: In the innovative laboratory of Nuvera Fuel Cells, the VACON® NXP series contributes to evaluating the performance of E-45 and E-60 fuel cell engines for electrical mobility under authentic conditions.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Solar-powered river tours protect Krka National ParkCROATIA: Two fully-electric, solar-powered vessels powered by Danfoss drives ensure silent, sustainable tours through the waterways of the spectacular Krka National Park in Croatia.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Future of the Fjords meets 2026 emission targets, todayThis world-first fully-electric carbon fiber vessel safeguards the pristine Norwegian fjord environment, ensuring zero emissions.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VACON® drives power hybrid ferries 24/7NETHERLANDS: Passenger ferries bridge Amsterdam’s IJ River, keeping the city connected around the clock. Hybrid propulsion powered by VACON® drives ensures 24/7 uptime, smaller generator size, better air quality, less noise and easy maneuverability of the vessels.