• My Apps
    My Apps You will have the option to use My apps once you login.

How did this platinum mine reduce risk and cost using efficient motion control?

Thursday, August 12, 2021

SOUTH AFRICA: BMG Electronics used Danfoss drives to support DryTech International in its development of a unique wet screw feeder for use in a platinum operation comprising mine, processing plant, and smelter. This solution improves reliability with elegant synchronization free of servo motion control, reduces costs, and eases maintenance time too.

Learn how BMG Electronics used Danfoss drives to help DryTech International to develop a uniquely efficient wet screw feeder.

Challenge: Unusual material requires unique solution

DryTech International developed the wet screw feeder for this plant to deal with unusual characteristics of the material being processed from platinum group metals (PGMs), chrome and base metals. The material is extremely sticky, with a consistency like clay, and needed to be transferred smoothly into a dryer. In addition, this material is received not only from mines within the immediate area in Limpopo province, but also from mines in the Mpumalanga province of South Africa, more than 300 km away. During transit, some composites dry out, while others remain wet.

From a mechanical design perspective, the gears required for the feeder would be large-scale, posing some practical challenges when it came to physically fitting into the unit synchronization without the screws clashing. Larger gears would also substantially increase the costs of the wet screw feeders. Ease of maintenance was a further requirement by the plant. The throughput needed from the first wet screw feeder was between 30 and 40 tonnes per hour, with 15 tonnes per hour required for the second feeder.

Solution: Synchronized screw shafts

3D wet feeder model without guards 3D wet feeder model with guards DryTech wet screw feeder setup using FC 302 drives

DryTech built a trial machine to test the application, and the trial showed that a three-screw shaft was the most effective solution. Although during the trial, the three screw shafts were mechanically linked to one other, the client favoured a solution with independent shafts, electronically synchronized using VLT® AutomationDrive FC 302 units controlling a 22 kW motor/gearbox on each shaft. This was a critical requirement, as all three independent shafts need to rotate in a coordinated manner to help prevent mechanical damage. For example, should one of the motors, gearboxes or shafts become overloaded and slow the motor down, it must be detected by an out-of-synchronization function and all screw shafts stopped. Once the problem is cleared and the application brought back manually, then the application automatically reverts back into the correct synchronized position at start-up, instead of having to return the shaft to a home position manually.

Stephen Brown, Mining Business Development Manager for Danfoss Turkey, Middle East & Africa

"The Danfoss VLT® AutomationDrive FC 302 offering provided the ideal solution for this client, due to its innovative alternative to the traditional servo control approach for positioning and synchronization operations. The drives are adaptable to the applications through simple parameterization.” explains Stephen Brown, Mining Business Development Manager for Danfoss Turkey, Middle East & Africa

During normal operation, the load on each drive is relatively light – at less than 50 percent motor full load torque (FLT) - but because of the sticky consistency of the material, there are times when higher loads occur. This has proven to be especially true during start conditions or low-feed rate conditions. The 22 kW drives with 22 kW motors are well suited to cope with these conditions, by constantly matching the power to the load. The motors are mounted above the gearbox driving each screw shaft, driving the gearbox via a belt drive.

“We needed the flexibility to be able to adjust the belt pulley ratio during commissioning in order to set the maximum speed, and therefore throughput rate, of the feeder. This also prevents mechanical damage at the belt, which will fail first.”

- Riaan Van Niekerk, DryTech spokesperson

Tighter speed and operation control

The final application set up by Juan Lerm, Field Service Technician at BMG Electronics, comprises three screws connected to the 22 kW motors and reducing gearboxes. The master motor (center motor) is controlled by a VLT® AutomationDrive FC 302 with PROFIBUS® and encoder options.The PROFIBUS® master is the plant control system controlling the operation and speed of this motor according to process requirements. The master motor is fitted with an encoder to increase its dynamic torque response, and the shaft of this motor has a reference encoder to measure the actual screw shaft rotational speed.

The higher the pulses per revolution (PPR), the better the syncing, as the increments are closer to each other, thus increasing the resolution of the feedback.

“In this application we used 8192 PPR multiturn absolute encoders,” explains Mick Baugh, Electronics Manager, Electromechanical Division, BMG. "When the wet feeder needs to run, it gives a ‘start’ command to the master variable speed drive (VSD) via PROFIBUS®. The master VSD then gives the start signals to the follower VSDs.”

The two follower screws are connected to VLT® AutomationDrive FC 302 with a VLT® Synchronizing Controller MCO 350 option also with PROFIBUS® for monitoring purposes. The master encoder is connected to both the MCOs as a master reference, which means that the MCO 350 cards monitor the speed of the master shaft. The follower encoder is fitted on the screw shaft of the follower screws, and these encoders are connected to each respective MCO as a feedback signal.

Electrical diagram of the application
Electrical diagram of the application

“The way this works is that the follower effectively mirrors the master encoder: if the master screw shaft runs at a certain speed, the follower MCO card monitors that speed and matches it so that the follower shaft is running in sync with the master reference,” states Baugh.

“If the application stops in an alarm state, all the motors will coast to a stop, and the follower shafts will be out of sync. When a start command is given, the master VSD has a five second delay, so that the screws will ramp up, and the application goes back into sync by itself. The master will then ramp up to the speed reference as per the PROFIBUS® signal.”

If maintenance has been done on the application, the screws will be out of sync. A manual sync was programmed so that the VSDs will go into a second setup, and now each screw can be jogged in forward and reverse to put all the screws back into a sync position. Once the screws are correctly aligned, the technician simply pushes the sync button to give the drive a new zero position. When the application starts up again it will run in sync.

“The fact that the Danfoss VLT® Synchronizing Controller MCO 350 option did not require the writing of a special APOS program was also a significant deciding factor,” Baugh adds.

Discover the ways in which intelligent drives add value to your operations:
VLT® AutomationDrive FC 302
Learn more about increasing productivity with Danfoss synchronization, positioning, and cam control Discover more drive solutions for significant CAPEX and OPEX savings in mining and mineral processing
Visit the FC 302 webpage Read the Motion Control brochure Read the Mining brochure

Related applications

Related case stories