• My Apps
    My Apps You will have the option to use My apps once you login.

Maximum power for excavating uphill tunnels

Monday, August 15, 2022

FRANCE: Powerful VACON® NXP drives power the Tunnel Boring Machine (TBM) used in construction of a new hydroelectric power plant in the Alpe d’Huez region. The Italian contractor Cogeis operates this TBM to dig a tunnel with a 22% gradient. It’s part of an innovative project which will deliver 100% renewable energy to the grid.

The hydroelectric power plant will integrate perfectly into the landscape, thanks to almost entirely underground systems. Tunnelling in this region requires the use of cutting-edge construction techniques, capable of overcoming the challenges posed by working in the difficult alpine environment, without disrupting the local tourism industry.

The challenge

For this project, Cogeis supplied a fully refurbished tunnel boring machine.

Paolo Bresciano, Technical Manager of the project, explains: “In this case, we had to dig uphill, with a considerable slope that significantly impacts the distribution of the forces at work in the 600-ton machine. Not only that, but because of the very limited space available at the access points to the construction site, about 25 m, we also had to invent a suitable way of assembling the 176 m long machine."

"There were many challenges to deal with, but in particular the electrical challenges led to a total rebuild of the equipment, which allowed us to obtain performance and flexibility far superior to that possible with the original configuration."

The TBM purchased by Cogeis used a configuration of 5 motors of 225 kW each, connected to a gearbox through clutches, to drive the rotating head.

The solution

“Because we wanted to keep the original motors designed specifically for this TBM, the solution proposed by Danfoss and DrivePro® Service Partner Gatta Srl is based on VACON® NXP Liquid Cooled drives, which have a very simple and effective load sharing management capability,” explains Paolo Bresciano.

“The drives control allows us to choose the rotation speed of the cutter with maximum flexibility, based on the expected conditions of the rock in the various stages of excavation progress.”

The motors were not originally designed for use with AC drives. Therefore, specially designed dU/dt filters were integrated to optimize motor control. Construction of the electrical panel was designed by engineers from Danfoss Drives Italy, who delivered all equipment ready to be installed on the TBM.

In addition, Danfoss provided DrivePro® Extended Warranty services, giving a warranty extension of up to 6 years, the longest in the industry.

The outcome

Construction of the complex La Sarenne project is currently in full swing, and excavation of the tunnel has started under the best conditions. The Cogeis TBM runs under the thrust of Danfoss drives. Upon completion of the tunnel, it will be extracted from the top and disassembled, ready to face new challenges. Thanks to the flexibility of the drive solution, it can be quickly prepared for transport to a new excavation site.

In 2024, the Compagnie Nationale du Rhone will be ready to feed 36 GWh 100% renewable energy into the grid annually, equivalent to the electricity consumption of 16,000 families.

Efficient tunnel boring

How does the contractor Cogeis dig a tunnel uphill at 22% gradient, with full reliability?

Products and services in this case story

Related solutions and applications

Related case stories

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Maximum power for excavating uphill tunnels

    FRANCE: Powerful VACON® NXP drives power the Tunnel Boring Machine (TBM) used in construction of a new hydroelectric power plant in the Alpe d’Huez region. The Italian contractor Cogeis operates this TBM to dig a tunnel with a 22% gradient. It’s part of an innovative project which will deliver 100% renewable energy to the grid.

  • if (isSmallPicture) { The fans of the Doha Metro achieve – maximum energy efficiency and reliability; } else if (isBigColumns) { The fans of the Doha Metro achieve – maximum energy efficiency and reliability } else { The fans of the Doha Metro achieve – maximum energy efficiency and reliability }
    The fans of the Doha Metro achieve – maximum energy efficiency and reliability

    Tailored for HVAC, flexible, modular and adaptable applications, the frequency control has played a key role in the ventilation system. It was the perfect fit, both in terms of EMC requirements, safety, harmonics, long cable lengths and dimensions, as well as its ability to function in temperatures of up to 50°C without loss of power.

  • if (isSmallPicture) { Copenhagen Cityringen – Tight spaces made manageable; } else if (isBigColumns) { Copenhagen Cityringen – Tight spaces made manageable } else { Copenhagen Cityringen – Tight spaces made manageable }
    Copenhagen Cityringen – Tight spaces made manageable

    Cityringen brings a new, completely automated underground line to the center of the Danish capital.

  • if (isSmallPicture) { High-performance tunnel ventilation despite long cables; } else if (isBigColumns) { High-performance tunnel ventilation despite long cables } else { High-performance tunnel ventilation despite long cables }
    High-performance tunnel ventilation despite long cables

    800 m of unscreened motor cable, interference free? Micheville Tunnel used VLT® HVAC Drive to achieve a high-efficiency, low-harmonic solution featuring exactly this. They even reduced costs by eliminating a voltage booster transformer.

  • if (isSmallPicture) { Reliable and effective ventilation in Ceneri Base Tunnel; } else if (isBigColumns) { Reliable and effective ventilation in Ceneri Base Tunnel } else { Reliable and effective ventilation in Ceneri Base Tunnel }
    Reliable and effective ventilation in Ceneri Base Tunnel

    By controlling fan speed in the Alps tunnel, VACON® NXP drives help enhance safety and energy savings.

  • if (isSmallPicture) { Safe and reliable ventilation in Sellero tunnel; } else if (isBigColumns) { Safe and reliable ventilation in Sellero tunnel } else { Safe and reliable ventilation in Sellero tunnel }
    Safe and reliable ventilation in Sellero tunnel

    VLT® HVAC Drives control fan speed to keep the tunnel constantly well ventilated and ensure clean air in an escape tunnel in the event of fire.