GLOBAL: Electrification and hybrid solutions are now booming. One of the first pioneers was the Dutch based energy storage manufacturer Alfen B.V., which has used Danfoss power conversion equipment since the early days. Alfen is a system integrator of smart plug and play energy storage solutions (ESS). Equipped with an integrated microgrid and energy management system (MEMS), Alfen systems are suited to both on- and off-grid containerized solutions with stackable units with capacity up to 100 MW.

Discover reliable ESS solutions
Support for renewable energy and electric vehicle rapid charging projects

Alfen and Danfoss Drives have installed numerous ESS solutions around the globe. Typically, these ESS sites are located off-grid, supporting production processes in parts of the world without stable electricity grids or powering temporary sites such as festivals. Other common applications are load balancing and energy trading. Let’s take a closer look at some of these projects.

Storage Solar Global
Czech Republic: The Czech solar PV company Solar Global selected Alfen to supply a 1 MW energy storage system connected to its Prakšice solar PV farm. The system was delivered in the fourth quarter of 2017 as the first large scale storage system in the Czech Republic.
Prepared for the future with storage
Solar Global develops and services solar photovoltaic (PV) farms and rooftop PV installations, and currently has some 100 MW capacity under service. As Solar Global wants to play an important role at the forefront of the energy transition, it is investing in an innovative energy storage solution
that initially will be used for energy trading. As the local market further develops, the system is also ready for other applications, such as providing grid stability services.
This project is supported by EU Regional Development Fund.

EV Peak shaving storage for Stedin and Mistergreen
The Netherlands: A project in which a rapid charging station for electric vehicles was equipped with solar panels and a local energy storage battery system was started in 2016. Project partners Alfen (energy storage systems), Stedin (grid operator) and MisterGreen (EV lease) have evaluated this pilot to be a success: peak loads decreased, maximum flexibility in offering variable price rates was attained, and the charging station itself became even more sustainable.
The number of electric vehicles is rapidly expanding, creating a need for more charging stations. In 2013, MisterGreen built the rapid charging station ‘Haarrijn’ at the A2 highway between Amsterdam and Utrecht. The pilot station with solar panels and local energy storage was commissioned in 2016. These solar panels provide the charging station with energy. If no vehicles are connected, the generated energy is diverted into the energy storage system, to be used when electric vehicles do connect to charge. This enables maximum usage of sustainably generated energy. Should the solar panels and battery run out of energy, the system can of course always fall back on the central grid.
More about Hybridization
- 
                
if (isSmallPicture) {   Drives for marine power conversion and generation Drives for marine power conversion and generationDraw upon expertise from Danfoss to optimize energy storage solutions using drives for power conversion both on board vessels, and in shore power supply for quieter and cleaner harbors. 
- 
                
if (isSmallPicture) {   Industrial DC backup ensures no more voltage dips Industrial DC backup ensures no more voltage dipsAchieve maximum uptime even during grid disturbances. Flexible targeted battery-based industrial DC backup solutions direct power supply to the most critical loads. These solutions support a combination of different energy storages to ensure a stable power supply when the national grid is unreliable, and ensure continuous running or controlled ramp down when required. 
- 
                
if (isSmallPicture) {   Intelligent power conversion for smart grids Intelligent power conversion for smart gridsBalancing supply and consumption is a complex task in a distributed smart grid, and this is where Danfoss supports you with certified power conversion solutions, saving you time, cost and effort in testing and certification. 
Products
- 
                        
if (isSmallPicture) {   VACON® NXP Grid Converter VACON® NXP Grid ConverterAir- and liquid-cooled drives specifically designed for smart grid, energy storage, green hydrogen, power conversion and marine energy management applications. 
Related Case Studies
- 
                    
if (isSmallPicture) {   Unlocking efficiency with a drive retrofit at a Czech hydropower plant Unlocking efficiency with a drive retrofit at a Czech hydropower plantCZECHIA: When 80-year-old gears were replaced by variable speed control at the Albrechtice hydropower plant, power production increased by 10%. 
- 
                    
if (isSmallPicture) {   Revolutionizing green hydrogen production with Danfoss Drives Revolutionizing green hydrogen production with Danfoss DrivesDENMARK: The Everfuel HySynergy facility produces green hydrogen with the help of iC7-Hybrid power converters for efficient, cost-effective electrolysis. 
- 
                    
if (isSmallPicture) {   Danfoss powers high-capacity SmartGrid energy storage Danfoss powers high-capacity SmartGrid energy storageNETHERLANDS: Retaining 80% capacity after 8000 cycles, SmartGrid smart battery containers promise 21 years of daily discharge and recharge without performance concerns. 
- 
                    
if (isSmallPicture) {   Speedy AC drive retrofit for Linz Strom Speedy AC drive retrofit for Linz StromAUSTRIA: A Linz Strom power plant needed to replace three ageing AC drives. DrivePro® Life Cycle Services played an essential role in meeting project requirements. 
- 
                    
if (isSmallPicture) {   Generating energy from green waste to fuel a city Generating energy from green waste to fuel a cityAUSTRALIA: Jeffries Group supports the city of Adelaide by using the biochar byproduct of green waste to generate renewable energy, driven by VACON power conversion. There's enough power to run their entire green waste operation and feed surplus energy back into Adelaide’s power grid — with zero emissions. 
- 
                    
if (isSmallPicture) {   Unique heat recovery for geothermal power using VACON® drives Unique heat recovery for geothermal power using VACON® drivesAUSTRALIA: A geothermal power station recovers energy during the bore water cooling process then uses it to generate power for the local community, with the help of VACON® drives.