• My Apps
    My Apps You will have the option to use My apps once you login.

Pressure concepts keep North Carolina's sweet potatoes ready for market and protect investments worth millions of dollars - with Danfoss valves

Wednesday, August 10, 2016

Located in Charlotte, North Carolina, Pressure Concepts is one of the state's leading providers of high-pressure solutions for a wide variety of industries. One of the firm's specialties is humidification solutions. Pressure Concepts has cooperated with Dr. Michael Boyette since the 1980s, and has produced hundreds of negative pressure ventilation storage facilities throughout North Carolina.

Sweet potatoes are increasingly popular in the United States, and North Carolina's farmers now produce about half of all the country’s crop. Although the sweet potato looks like an orange version of its more popular namesake, they are not actually of the same genus as the common white potato. In fact, they are far more difficult to store than regular potatoes.

If sweet potatoes are stored at too low humidity, they dry out and become inedible. It the humidity is too high, they rot. For years, this meant that the year’s crop had to be sold out within a few months of harvest. Farmers flooded the market so as not to be stuck with unsaleable product, and prices tumbled as supply outstripped demand. If only there were a way to increase the storage ability of the sweet potatoes, then farmers could sell their harvest throughout the year and earn higher profits as supply dwindled.

Dr. Michael Boyette, a researcher at North Carolina State University, found a way when he revolutionized sweet potato storage with negative pressure ventilation and constant temperature and humidity control. Pressure Concepts, Inc., a leader in high pressure solutions for many industries in North Carolina, worked with Boyette from the start.

Related products

Download case as PDF