Every day, the food processing industry is investing in solutions that are more and more focused on safety and on the reduction of the charges of ammonia and losses in their plants. Cataby, a pork producer in Brazil, has recently relied on the expertise of SCE Engineering for designing and installing a 4,000-meter-squared distribution center equipped with an ammonia refrigeration system in Santa Bárbara D'Oeste, the countryside of São Paulo.
SCE came to Danfoss to support them and the proposed solution was to install Flexline™ ICF valve stations, designed to offer intelligent simplicity, time-saving installation and advanced flexibility. By adopting Danfoss solutions, they could reduce at least 15% of the welding points and 10% of the installation hours according to Sérgio Santos, SCE engineer.