When an aging reciprocal pump suddenly failed at a Cabo San Lucas resort, Gemini Water Systems recommended a new Danfoss APP to replace it. The retrofit would be the first time an axial piston pump was installed in a region long dependent on reciprocating pumps for SWRO.
The short lead time to source and install the new pump initially caught resort managers' interest. But the most convincing reasons for the decision were radically simplified maintenance routines and lower total costs of ownership.
The challenge: Replace an old pump fast, and keep the water flowing at a busy resort
Located at the southern end of the arid Baja Peninsula, the Los Cabos region is Mexico's fastest-growing tourist destination. Pueblo Bonito Sunset Beach Golf & Spa Resort, a popular luxury resort, is located at the very tip of the peninsula by Cabo San Lucas, the area's biggest city. Like practically everywhere else in the desalination-dependent region, the resort's SWRO plants used reciprocating pumps to supply the high pressure. Until recently.
"Los Cabos has traditionally been dominated by reciprocating pumps," explains Dean Bedford of Gemini Seawater Systems. "In terms of SWRO, it's a conservative market that has not been very open to change. So, when Pueblo Bonito Sunset Beach needed to replace a failed pump fast without disrupted service, it was Danfoss' relatively short lead times that initially enabled us to get the APP onto their radar. This opened the door to more important long-term considerations, not least maintenance and TCO."
The solution: The first Danfoss APP pump in Cabo San Lucas
Gemini Seawater Systems has built its business on designing and modernizing SWRO plants with the lowest possible life-cycle costs. Practical field experience, premium components, and a relentless focus on training local maintenance personnel are all key elements of its success.
"Best-in-class components are an essential part of our approach," says Bedford, "but what really sets us apart is the importance we place on understanding local operational contexts and training and communicating with the people who will actually be responsible for plant operations and maintenance. These are the things that ultimately make or break a plant's success, so integrating operations into plant design and TCO calculations just makes good sense."
"The Danfoss APP removes a lot of unknowns from the maintenance equation. Will staff remember lubrication schedules, or won't they? Will they keep an eye on belts and the pump's vibration effects on other system components? With APPs, we reduce the number of things that can go wrong and really simplify maintenance. We also save serious money on energy costs. Both things go hand in hand with our business model – and with our customers' long-term interests."
![The results: Quick retrofit with long-lasting benefits](/media/5305/get-more-with-less-by-retrofitting-reciprocal-pumps-with-danfoss-app-pumps-danfoss-1.jpg?anchor=center&mode=crop&width=520)
The results: Quick retrofit with long-lasting benefits
Working closely with their local partner in Cabo San Lucas, Polymetrics, the retrofitted pump was installed within weeks instead of months.
"The new Danfoss APP 26 pump runs 24 hours a day, producing 117 gallons per minute," says Joseph E. Rafferty, president of Polymetrics. "It takes just half the space of its predecessor and is also much quieter, something the resort is particularly happy about. But they're even happier about all the electricity they're saving day in and day out."
Dean Bedford is convinced that the APP 26 will not be the last installed in Cabo San Lucas. "When most of the region's the big plants went online years ago, the APP pump line-up was either non-existent or still so small that they couldn't produce the necessary volumes. Things have changed, and axial piston technology is now providing pressure for systems producing up to 88 m3 per hour. I believe the Danfoss APP is the pump of the future – also in Cabos San Lucas."
For more information about Gemini Seawater Systems LLC, please visit: https://www.geminiseawatersystems.com/
For more information about Polymetrics, please visit: http://www.polymetricsmx.com/
Read more about Danfoss APP high-pressure pumps for reverse osmosis applications
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }High-pressure pumps for SWRO applicationsThe range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.