Flue gas heat recovery to enhance sustainable heating for Frederikshavn residents

  • Overview
  • Related products
  • Related applications
Wednesday, August 21, 2024
Frederikshavn

At Frederikshavn District Heating Utility (DHU), a 14 MW gas boiler is utilized during the cold months to ensure sufficient heat supply to the Frederikshavn community. A project was initiated by ME Production, involving Danfoss and heat pump OEM partner Energy Machines, to enhance energy utilization by recovering boiler flue gas heat. This was accomplished by modifying the existing economizer to increase the recovered capacity and boost boiler capacity with the resulting condensing function. A heat pump is integrated into the system to boost the heat from exhaust recovery back to the boiler. This initiative reduces operating costs and significantly contributes to CO2 emission reduction.

As a result, Frederikshavn DHU can expand its existing heat production infrastructure while also reducing overall heat generation operating costs.

Introduction

Frederikshavn DHU operates a 14-megawatt gas boiler to provide essential heating services during colder periods. To improve energy efficiency and reduce environmental impact, a project was initiated to recover more energy from the flue gas emitted by the existing biomass boiler system.

Frederikshavn utility

Problem/Challenge:

The main challenge was to maximize energy recovery from the flue gas and enhance the overall efficiency of the heating system, driving down operating costs and the end customer heat price. This required significant modifications to the existing economizer and integrating advanced heat pump technology.

Heat pump

Solution:

The solution involved rebuilding the economizer to recover heat from the exhaust in a closed chilled water heat pump evaporator loop. This recovered heat is then boosted through the heat pump to pre-heat the feedwater entering the boiler, thus reducing the boiler’s workload. The flue gas condensing recovery leads to a high heat pump chilled water temperature, which in turn results in a lower temperature lift requirement for the heat pump and a high resulting heat pump coefficient of performance of 5.7.

Heat pump front page

Results/Outcomes:

The project successfully enhanced energy recovery, leading to significant operational cost savings and a notable reduction in CO2 emissions. The estimated energy savings are equivalent to the annual heat consumption of 150 households. The project also marked ME-Production’s significant entry into the land-based market, demonstrating the effectiveness of their heat pump technology.

It’s inspiring to see how collaboration helps develop new, innovative solutions and ultimately sends greener heat to the residents of Frederikshavn. We must deliver on the green transition, and therefore we need skilled companies like ME Production that have the courage to think outside the box and develop and design entirely new green solutions.

Mayor Birgit S. Hansen, Frederikshavn Municipality

Implementation:

The project was implemented through a collaboration with Energy Machines and ME-Production. Energy Machines integrated a range of Danfoss solutions into the water-water heat pumps, including Turbocor® compressors and other essential components.

Machines is unique in utilizing a full portfolio of pre-configured Danfoss component solutions for their heat pumps. ME-Production managed the contract with Frederikshavn Forsyning and oversaw system design and control. The project also featured the first use of the new Alsmart™ controller, which was specifically programmed for this application.

Conclusion:

The Frederikshavn DHU Flue Gas Condensing Heat Recovery Heat Pump project highlights the benefits of strategic collaboration and advanced technology in achieving energy efficiency and environmental sustainability. This project’s success sets a benchmark for future initiatives in both the district heating and maritime sectors.

Download the full case study

Related products

  • if (isSmallPicture) { ICM Flexline™ motor valves - Danfoss; } else if (isBigColumns) { ICM Flexline™ motor valves - Danfoss } else { ICM Flexline™ motor valves - Danfoss }
    ICM Flexline™ motor valves

    The ICM motor operated valves from Danfoss ICV Flexline™ series are quick and simple to handle, install and service due to their low weight and compact design.

  • if (isSmallPicture) { EVR solenoid valves, direct or servo operated; } else if (isBigColumns) { EVR solenoid valves, direct or servo operated } else { EVR solenoid valves, direct or servo operated }
    EVR® solenoid valves, normally open (NO) or closed (NC)

    Danfoss offers a complete range of direct and servo-operated solenoid valves for air conditioning and refrigeration systems. The easy-to-service EVR® valves can be used in liquid, suction and hot gas lines. The valves are compatible with fluorinated refrigerants, including high-pressure refrigerants such as R410A (EVRH).

  • if (isSmallPicture) { ETS electric expansion valve - Danfoss; } else if (isBigColumns) { ETS electric expansion valve - Danfoss } else { ETS electric expansion valve - Danfoss }
    ETS electric expansion valves

    ETS is a series of electric expansion valves for precise liquid injection in evaporators for air conditioning and refrigeration applications. The valve piston and linear positioning design is fully balanced, providing bi-flow feature as well as solenoid tight shut-off function in both flow directions. ETS valves are compatible with electronic control solutions from Danfoss and other manufacturers.

  • if (isSmallPicture) { GBC shut-off ball valves - Danfoss; } else if (isBigColumns) { GBC shut-off ball valves - Danfoss } else { GBC shut-off ball valves - Danfoss }
    Shut-off ball valves for refrigeration, GBC

    GBC ball valves are manually operated shut-off valves suitable for applications where bi-directional flow is a requirement.  GBC valves are approved for applications in liquid, suction, and hot gas lines in refrigeration and air conditioning systems.

  • if (isSmallPicture) { AKS4100 liquid level sensors  - Danfoss; } else if (isBigColumns) { AKS4100 liquid level sensors  - Danfoss } else { AKS4100 liquid level sensors  - Danfoss }
    Liquid level sensors

    The AKS 4100 liquid level sensor takes you to a whole new level of flexibility and accuracy. With TDR guided radar technology, the sensor is fully adapted to industrial refrigeration – reliable and with high accuracy.

Related applications