Banja Luka is the second largest city in Bosnia Herzegovina. The city’s district heating utility, Banja Luka Eko Toplane, is constantly looking for ways to make heat production, distribution, and consumption more energy efficient while improving comfort for its 20,000 end users. In 2017, as part of its decarbonization goals, the city of Banja Luka and Eko Toplane introduced a new renewable heat source for the district heating system, wood biomass, and set the stage for an ambitious renovation project.

The Challenge: Renovate 34 of the city’s largest heating substations
Switching to renewable energy sources was just the beginning. To create lasting energy efficiency improvements, Eko Toplane and the city of Banja Luka knew they needed to optimize their heating substations. The District Heating Utility selected 34 of its heating substations for optimization. The substations have an installed capacity of 57 MW and provide 25% of the district heating system’s total heat and flow.

The Solution: Danfoss Leanheat® Monitor enables full substation digitalization
Danfoss worked with Eko Toplane from the project’s early stages, helping them to select the heating substations for renovation, choosing the appropriate equipment and handling installation and commissioning. Once the renovation was complete, Danfoss connected all the heating substations to Leanheat® Monitor, so utility managers could monitor, control and maintain substations remotely. At one of the heating substations Danfoss also installed its Titan™ substation application, which uses groundbreaking digital twin technology to ensure correct commissioning, enhanced performance and the lowest possible return temperature.

One of this project’s biggest achievements was equipping Banja Luka with the skills and tools they need to manage future efficiency and transformation projects. We worked with the team to give them the support and guidance necessary, so they would be able to install, connect and commission the equipment independently.

The Results: reduced heat consumption by 10%
The renovated heating substations are now more balanced in terms of available flows and pressures so they can operate efficiently under local conditions. Thanks to Leanheat® Monitor, utility managers can remotely monitor and manage each heating substation, which has reduced the number of callouts and associated costs. They are also able to carry out predictive maintenance and respond more quickly to system warnings and alarms.
The project met all objectives, including laying the groundwork for new users to be connected to the district heating network and digitalizing the entire system. The District Heating Utility has also started implementing optimization modules and algorithms to manage heat production and distribution, and autonomously operate heating substations to ensure they perform optimally with the lowest return temperature.
These combined measures have resulted in an annual energy saving of 10%.

New projects on the horizon
The city of Banja Luka and the district heating utility have recognized Danfoss as a strategic partner in the field of district energy – advanced components supplier, solution provider, and aftersales support. The next step in the partnership is a project to renovate, digitalize, and optimize 100 new heating substations and improve the entire system operation using advanced optimization tools. The District Heating Utility is also implementing Leanheat® Network, Danfoss’ thermo-hydraulic modeling tool developed specifically to help district heating utilities optimize the design and operation of district energy distribution systems.

We can say that Danfoss has become a strategic partner of Eko Toplane Banja Luka, and that this is a success story and an extraordinary cooperation that should be characterized as a win-win, because this is the only way to guarantee further technological development that leads towards even better energy efficiency.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Titan™ by DanfossThere’s nothing like perspective. Looking at something differently allows you to see new things. It adds dimension. To the digital dynamics of your network. The pulse of the grid. Danfoss Titan™ combines best-in-class substations with innovative digital twin technology to add a new and data-driven dimension to district energy.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }SubstationsSubstations are house heating systems or units in apartments that handle heat transfer from district heating pipes into your home to get hot water and heat on demand.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Differential pressure, flow and temperature controllersBalance your network, save energy and improve end-user comfort by hydronic balancing and control of district energy networks. Optimal hydronic balance and perfect temperature control are the key to maximizing the efficiency of heating or cooling networks.