• My Apps
    My Apps You will have the option to use My apps once you login.

Danfoss’ Leanheat® Building helps Avain deliver energy-efficient heating to residents throughout Finland

Thursday, December 15, 2022

Avain has installed Danfoss' modern SCADA solution, Leanheat® Building in over 100 new and renovated residential properties containing nearly 3,000 apartments.

Leanheat® Building uses data provided by sensors installed in the apartments to learn each building’s thermodynamics and optimize the heating accordingly. The software also adapts the heating system to changes in weather conditions and in the building’s characteristics as it ages. By fine-tuning the heating network and district heating demand response, Leanheat ensures apartment blocks and terraced houses have the highest possible energy efficiency at all times.

According to Jan Bertills, Director of Real Estate at Avain, the Leanheat® Building system offers benefits for building residents and managers.

“In 2018, we started a pilot project which showed that the Leanheat® Building can save up to 10% of the energy used for district heating annually.This is good news for residents, as they benefit from a constant temperature and savings on heating costs. This, in turn, leads to lower management costs and lower heating bills. In these times of energy scarcity, we all need to save energy and, by extension, the environment," he says.

Kimmo Bister, Account Manager in the Danfoss Leanheat® Building team, also sees the cooperation as fruitful.

“It was clear from the start that the purpose of our cooperation with Avain Companies was to improve living comfort and reduce energy consumption. Achieving these goals required open communication between both parties, and and we’ve experienced that throughout this project. As the Leanheat team is part of Danfoss' international network, it also gives us the opportunity to continuously bring new, innovative solutions to property owners, that we can then tailor to their specific needs. It’s a priviledge to be part of Avain Companies' energy efficiency strategy.”

Leanheat® — For true energy optimization. From people to production.

Buildings account for a staggering 40 percent of the world’s energy consumption. And in Europe alone, almost a third of residential heating comes from fossil fuels.
Leanheat empowers district energy networks to optimize the operational efficiency of buildings and increase the comfort of end-users through end-to-end software solutions.