• My Apps
    My Apps You will have the option to use My apps once you login.

Pro-FX® Configure Software

  • Overview
  • Current Downloads
  • Prior Revisions
  • Documents

Pro-FX Configure v2 is valve configuration software the way it should be: smarter, faster, easier. Featuring a wizard-based setup as well as parameter-based tuning, the user-friendly software enables quick and easy configuration of advanced AxisPro® valves.

A streamlined, step-by-step workflow takes the user through valve setup for specified control modes including spool position, cylinder position, pressure, speed, or force. The program simplifies everything from setup to tuning and commissioning, helping you get the machine to the customer faster.

Features

  • 100% wizard-based setup
  • Parameter-based tuning
  • Expanded, improved alert library for diagnostics
  • Identifies firmware version and prompts update
  • Enhanced data plotting to help tune the application
  • No need to tune PID controller for most applications, saving time
  • Support for legacy versions of AxisPro firmware (7.x and 107.x)
  • Updated User Guide available on software download webpage
  • Updated release notes and known issue list included with software

AxisPro Valve Compatibility:

Model codes ending in -002-10: This version of Pro-FX is compatible with all valves having model codes ending with -002-10.

Model codes ending in -004-11: This Pro-FX version MUST be used to configure valves with model codes ending with -004-11.

 

For support inquiries, please send us an email.

Prior Revisions

Supported CAN Card Drivers and Ethernet Tools

Below is a list of 3rd party drivers and tools used to configure and connect to devices supported by Pro-FX Configure.

Note: Driver versions newer those tested against Pro-FX Configure may not run correctly with Pro-FX Configure.

Vendor Danfoss
Website Software and Tools
Used by Pro-FX Configure Platforms AxisPro, CMA
Version Installed by and Tested Against Pro-FX Configure v2.2.1.0
Installation Notes This is installed as a part of PLUS+1 Update Center. To get updated drivers install PLUS+1 Update Center. Click "Select Files Manually". Click "Edit". Then select CG150 under Files/Drivers. Install as usual with Update Center.
Vendor CANCapture
Website https://www.cancapture.com/cancapture
Used by Pro-FX Configure Platforms AxisPro, XFX
Version Installed by and Tested Against Pro-FX Configure v3.3.0.0
Installation Notes Download the latest driver from the section entitled “Latest Driver Installation.” This will download the driver installation program. Run the program after it's downloaded.
Vendor

Hilscher

Website

https://hilscher.atlassian.net/wiki/spaces/ETHDEVCFG/overview

Used by Pro-FX Configure Platforms AxisPro
Version Installed by and Tested Against Pro-FX Configure v1.0900.3.5506
Installation Notes Click the download link for the "current release" and follow the download instructions on the page you're brought to.
Vendor

Kvaser

Website https://kvaser.com/download/
Used by Pro-FX Configure Platforms AxisPro, CMA, XFX
Version Installed by and Tested Against Pro-FX Configure v5.22.392.0
Installation Notes Click "Download" in the "Kvaser Drivers For Windows" section to navigate to the download page. Then download the version of the driver installation program you want (usually the most recent). Run the downloaded installation program.
Vendor

PEAK-System

Website Drivers: PEAK-System
Used by Pro-FX Configure Platforms

AxisPro, CMA, KBDG, KBFRG4, XFX

Version Installed by and Tested Against Pro-FX Configure v4.1.3.202
Installation Notes Click "Device Driver Setup Windows 11 (x86ARM64), 10 (x64)" to download a zip file containing the driver. Unzip the zip file then run the installation program.
Vendor

Softing AG

Website

Downloads | Softing

Used by Pro-FX Configure Platforms AxisPro, CMA, XFX
Version Installed by and Tested Against Pro-FX Configure v5.21
Installation Notes Select from the lists presented on the webpage. First, select the following in the three list boxes from left to right: 1) CAN/CANopen 2) USB and Bluetooth Modems 3) CANpro USB – CAN Single Channel USB Interface Card. Next click the “SHOW” button under the “Product” list. Then click the Windows Driver link. It will resemble the following: “CAN Driver, API, Manual, LeanCANopen Programming Samples Windows 10/Windows 8/Windows 7 V5.23.1”.  You will be prompted to login before you can download the driver.
Vendor

Intrepid Control Systems

Website Support Resources | Intrepid Control Systems, Inc. (intrepidcs.com)
Used by Pro-FX Configure Platforms AxisPro, KBDG, KBFRG4
Version Installed by and Tested Against Pro-FX Configure v3.9.14.15
Installation Notes Click the link named "ICS Hardware Installation kit" to download a zip file containing the driver installation program. Unzip the file and run the installer.

Documents

Documents
Type Name Language Valid for Updated Download File type
Fact sheet Vickers by Danfoss Pro-FX Configure v2 - Where configurability meets simplicity fact sheet English Multiple 13 Nov, 2023 1.3 MB .pdf
User guide Vickers by Danfoss Pro-Fx Configure v2 Software user guide English Multiple 25 Oct, 2023 3.1 MB .pdf