![Drinking water production](/media/2106/drinking-water-production.jpg?anchor=center&mode=crop&width=520)
Drinking water production
Whether surface water or groundwater is used for water production, Danfoss AC drives can help optimize the process and reduce energy and maintenance costs. A typical application is the control of deep well pumps, where the integrated advanced minimum speed monitor secures sufficient lubrication to protect the pump. Energy savings are achieved by selecting wells based on water level height. The VLT® AQUA Drive is also widely used in the desalination industry for controlling inlet and high-pressure pumps as well as booster pumps in relation to energy recovery.
![Drinking water distribution](/media/2105/drinking-water-distribution.jpg?anchor=center&mode=crop&width=520)
Drinking water distribution
Within the water supply, drinking water distribution is typically the largest energy consumer. At the same time, 25–50% leakage is not unusual. By dividing the water distribution into pressure zones, the average pressure can often be reduced by 30–40%. The VLT® AQUA Drive is very widely used in boosting pumping stations to regulate pressure in each pressure zone. Integrated application software functions, such as Sleep mode, Dry run detection, Automatic Energy Optimization (AEO), Cascade control, Automatic flow compensation and Ramp functions help simplify the installation and make it more reliable, reduce the risk of water hammer, control pressure and reduce energy consumption.
![Irrigation](/media/2101/irrigation.jpg?anchor=center&mode=crop&width=520)
Irrigation
With access to water resources becoming scarce in some regions of the world, efficient and sustainable irrigation is becoming more and more important. It’s all about supplying enough water to get maximum crop yield without using more water and energy than absolutely necessary. Danfoss AC drives adapt pressure or flow rate to the actual need. And integrated application software functions help to both protect the pipe system by limiting pressure boost and cut energy consumption.
The ultimate solution, and a very fast-growing trend, to reduce energy consumption is to use solar-powered pumps. Danfoss Drives has developed a dedicated inverter series exactly for this purpose. The VACON® product range includes a specially designed encapsulation for this environment and advanced software, meaning that operation is possible even when clouds are partially blocking sunlight from reaching the photovoltaic panels.
![Wastewater canalization system](/media/2103/wastewater-canalization-system.jpg?anchor=center&mode=crop&width=520)
Wastewater canalization system
Energy optimization and SCADA control of the wastewater canalization system is also a fast-moving trend. By using the VLT® AQUA Drive’s integrated deragging function, it is possible to improve pump efficiency by 15–30% and also drastically reduce maintenance costs. The deragging function prevents pump efficiency from dropping by increasing clocking and extends pump maintenance intervals. Using an AC drive together with a SCADA system also offers the possibility to secure maximum utilization of the volume capacity in the canalization system in relation to storm water overflow.
![Reduced leakage and energy consumption go hand in hand](/media/2102/reduced-leakage.jpg?anchor=center&mode=crop&width=520)
Reduced leakage and energy consumption go hand in hand
The energy used in the water distribution system typically represents 60–80% of the total energy consumption for the whole water supply system. By adapting the pressure to the real need using pressure zones and boosting pumping stations, you can achieve energy savings of 25–40%. At the same time, you can reduce water leakage by 30–40%.
Regulating the pressure in the network can also provide the following benefits:
- a 40–55 % reduction in the amount of new pipe breaks
- a reduction in maintenance costs and expensive pipe and road repair
- limited risk of bacteria and contamination of tap water (infiltration)
- extended service life of the network
- postponed investment in plant upgrades
- reduced risk of water hammer
![](/media/3889/pumps_1920x420_right.jpg?width=420&height=1920&rnd=131596277889000000?anchor=center&mode=crop&width=1920&height=420)
The Jurex seed company saves 35% on irrigation pump energy consumption
The Romanian seed company Jurex srl installs VLT® AQUA Drive frequency converters in its new irrigation pumping station.
Products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VACON® 100 FLOWDedicated functionality that improves flow control and saves energy in industrial pump and fan applications.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VACON® NXCAn enclosed drive designed for demanding applications that includes options for Active Front Ends and low harmonic solutions.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® AQUA Drive FC 202VLT® AQUA Drive FC 202 controls all types of pumps and comes equipped with a cascade controller.
Case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }How a new water pumping station keeps supply flowing in BernSWITZERLAND: The Wehrliau pumping station in Bern delivers up to 1.20 M liters of drinking water hourly. iC7 drives play a key role in ensuring reliable supply.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }How did Sincrondraiv SRL improve irrigation pumping efficiency by up to 40%?ROMANIA: Digitizing irrigation systems helps farmers achieve better harvests. Pumping stations now use 30-40% less energy and use water more efficiently too.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Carlsberg brewery drives down energy consumptionPOLAND: For more than a decade, Danfoss drives have reduced the power consumption at Carlsberg’s Okocim Brewery. The brewery uses less water and has lowered its emissions, too.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Koyambedu: 22% reduction in energy consumption at wastewater treatment plantINDIA: By using VLT® AQUA Drive FC 202 from Danfoss, Koyambedu wastewater treatment plant has reduced its energy consumption significantly.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Driving efficient life support systems at Lodz ZooPOLAND: The Lodz Zoo Orientarium uses high-efficiency VLT® AQUA Drive FC 202 to secure reliable water quality in life support systems for rare animal species.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Bringing clean drinking water to rural Kenya with 100% renewable resourcesKENYA: A solar-powered desalination plant in Kenya gives the community affordable, clean, and sustainable drinking water and irrigation water.
Contact us
For further information please contact us