Sustainable desalination with maximum energy efficiency
According to the UN, water scarcity is one of the major challenges facing the world today and tomorrow. The need to find sustainable solutions for new freshwater supplies is urgent; solutions that take the straight road from saline to fresh water at low cost and with minimum impact on climate and nature.
Due to its high energy efficiency and reliability, Sea Water Reverse Osmosis (SWRO) is one of the most sustainable and cost effective solutions for converting sea water to potable fresh water. At the same time, SWRO technology undergoes rapid development to improve energy efficiency and support large-scale freshwater production.
Features and benefits
Extremely low energy consumption
Ultra-low maintenance costs
Simple to operate
Minimal service and long service intervals
Small footprint but effective, compact and light in weight
Danfoss takes lead in SWRO innovation
Danfoss is committed to supporting the sustainable desalination industry with energy efficient SWRO solutions. The product offering includes four core technologies, comprising high-pressure pumps, AC drives, energy recovery devices and pressure and fluid control devices. These combine into highly efficient and lasting water purification solutions that return energy savings of up to 65% compared to traditional centrifugal pump systems without energy recovery devices and drives.

By land, by sea - anywhere
At large scale, reverse osmosis plants are capable of providing freshwater to entire cities while compact solutions are ideal for supplying hotels and resorts, ships, and offshore facilities with clean water.

Today’s challenge – Tomorrow’s opportunity
Water is vital for life. Shortage of fresh water has spurred innovation to find efficient and climate-friendly solutions that turn seawater into fresh, clean water.
Reverse osmosis is the leading technology. It is simple, reliable and requires less energy than other desalination techniques.

Creating a sustainable future with seawater
65% savings on your desalination systems with Danfoss high-pressure pumps, Danfoss pressure transmitters, Danfoss drives and Danfoss energy-recovery devices (iSave) compared to desalination plants with centrifugal pumps and without energy-recovery devices and drives.

Acciona and Danfoss create innovative SWRO
Technologically advanced solutions allowed Acciona to create an innovative sea water reverse osmosis (SWRO) modular desalination plant for the Sarlux refinery in Sardinia, Italy, reducing energy consumption compared to traditional solutions.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }DST P40I titanium pressure transmitter for use in corrosive environments and with aggressive mediaFor use in corrosive environments and with aggressive media, Danfoss offers the robust DST P40I pressure transmitter made of Titanium and with ceramic pressure sensing element. DST P40I is optimized for use in applications such as desalination systems, seawater cooling, and chemical processing.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }High-pressure pumps for SWRO applicationsThe range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Energy recovery device for medium to large SWRO applicationsThe first active ERD for medium and large plants integrates highly effective isobaric pressure exchangers with a low-voltage motor to eliminate the risk of rotor overspin, reduce mixing and biofouling, and facilitate smarter automation. Covering train sizes from 1,500 m3/day and above.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® AQUA Drive FC 202VLT® AQUA Drive FC 202 controls all types of pumps and comes equipped with a cascade controller.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }iSave® energy recovery devices for high-pressure membrane applicationsWith a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day
Case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Salt Separation chooses Danfoss for cruise ship SWRO retrofitSalt Separation Services boosted capacity by 75% and significantly reduced SEC by retrofitting a luxury cruise ship’s SWRO plant with a Danfoss APP pump and iSave ERD – all in the same tight space in the ship’s engine room.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }APP pumps with ceramic chosen for containerized solutionsWhen a Spanish engineering company needed one compact, reliable, and energy-efficient SWRO solution for three separate end users, Gefico’s engineers proposed a compact, modular train design that could be both containerized and built on skids. Danfoss’s ceramic APP pumps and iSave ERDs are at the heart of the seven trains that Gefico designed and produced
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }WatMan specifies Danfoss for the world’s largest cruise ship’s SWRO plantWatMan Engineering chose Danfoss high-pressure pumps and ERDs for the SWRO plant supplying fresh water to the world’s largest cruise ship, Icon of the Seas. The Finnish specialist will also use Danfoss technology for the next two Icon-class ships.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Peter Taboada tailors energy-efficient wellboat SWRO with flexible Danfoss technologyPeter Taboada works closely together with wellboat builders to deliver efficient, space-saving water-making solutions that boost ROI. Flexible Danfoss high-pressure pumps and ERDs play a key role in the company’s success.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danfoss components chosen to provide fresh water in emergency situationsMetis Water chose Danfoss APP pumps and iSave ERDs for its mobile 1,000 m3/d SWRO plant. Designed to fit inside a 40 ft container, the plug-and-play solution can quickly be deployed to supply fresh water in emergency situations – reliably and energy efficiently.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Koyambedu: 22% reduction in energy consumption at wastewater treatment plantINDIA: By using VLT® AQUA Drive FC 202 from Danfoss, Koyambedu wastewater treatment plant has reduced its energy consumption significantly.
Articles
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Brine mining and SWROThe mining of SWRO brine for valuable chemicals has begun – and has the potential to disrupt the entire SWRO industry.
In this blog, we examine what makes brine mining interesting for SWRO operators and provide an overview of the key issues that might affect its adaptation.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }How SWRO on wellboats helps marine salmon aquaculture stay healthy & profitableAquaculture is growing worldwide, and we now eat more farmed salmon than wild-caught.
Read our latest blog to learn how SWRO plays an innovative and important role in keeping salmon raised in marine aquaculture free from parasites through freshwater treatment on specially built wellboats.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Is it time for smarter SWRO maintenance?Maintenance of high-value assets is critical to mitigating operational risks. As the SWRO industry evolves, more owners and operators will transition from simple corrective and preventative maintenance strategies and increasingly apply data-supported insights to optimize performance and profits.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Desalination meets decarbonization: How renewable energy can power SWROThe world’s increased use of renewable energy sources has the potential to reduce SWRO’s carbon footprint and increase its affordability and availability.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }The four global trends that will impact desalination in 2022Energy efficiency has a minor impact on SWRO’s CAPEX but a huge impact on OPEX & TCO
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Retrofits: The key to energy efficiency, cost savings and decarbonization of SWRO’s installed baseDesalination plants can save money and CO2 by retrofitting older plants for optimal energy efficiency - isobaric ERDs and APP high-pressure pumps are the key
Contact us
For further information, please contact us.