Traction control technologies
Danfoss has made advances in traction control an integral part of our mission to help engineer tomorrow. This commitment has led to an advanced understanding of traction control technologies. These allow us to provide you with the products and solutions you need to make superior traction control a competitive advantage on your machines.
In off-highway applications, vehicles often encounter terrain with varying levels of friction. When working conditions are wet, muddy or icy, equipment operators need confidence that they will have proper traction control. This, to get the job done and keep them safe in their vehicle.
Oftentimes, a vehicle’s wheels are not all on the same type of surface. When this situation occurs, proper traction control technologies help manage wheel speed and keep the machine from excessively slipping.
One example of how Danfoss addresses this challenge is by utilizing hydrostatic drive systems. These are driven by H1 pumps, with H1 motors at each wheel. When low-traction situations are detected by wheel speed sensors, Danfoss microcontrollers control the displacement of each motor independently. The force applied to each wheel matches the amount of force that can be maintained by the current ground contact of the wheel. Resulting in reduction in ground damage and the maximum tractive force possible for the ground conditions encountered by the machine. This type of solution can be tested and refined for your specific traction control needs. This by using a variety of real-world testing conditions available at Danfoss Application Development Centers.
Related products
Coming soon...
Coming soon...
Related solutions
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Automotive control solutions
Automotive control technologies help increase machine controllability, regardless of operator skill level.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Best point control
This unique solution works by constantly adjusting operating parameters of key drivetrain components to maintain optimal efficiency points. These include the diesel engine, hydrostatic transmission, hydraulic pumps and motors.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Braking
Heavier vehicles. Smaller engines. Stricter stopping-distance regulations. They’re all challenges to heavy-equipment braking systems — and they’re all challenges that can be overcome with Danfoss solutions.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Dual Path
Today’s machines get more done, more efficiently, thanks to advances in transmissions, pumps and motors. Danfoss is leading the way in perfecting the dual-path solutions that bring them all together. Delivering precision equipment control, less operator fatigue and greater productivity.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Propel application library
The Danfoss Propel Application Library (PAL) is a collection of function blocks for propel applications.
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Total machine management
Our PLUS+1® platform delivers the software application development power you need — and doesn’t require specialized programming skills.