A unique supermarket
On June 29th the COOP 365 Smart Store opens for the public for the first time. In the Danfoss Smart Store the cooling and heating technologies are in operation 24/7. It’s not a laboratory simulating real-life operation. Customers open cabinet doors hundreds of times a day and every time it puts demand on the cooling and heating of the supermarket. The Danfoss Smart Store demonstrates our available solutions in action.
BALS, Brugsforeningen for Als and Sundeved, Denmark’s largest independent supermarket association, will rent the building from Danfoss and will install a COOP 365discount supermarket. BALS, which works together with COOP, has a total of 13 stores in the area around Sønderborg in Denmark and since 2015 has consistently reduced the consumption of energy in its stores. So far, they have cut 44 percent of their total CO2 emissions. Therefore, it was a natural next step that BALS became a partner in the project.
Lars G. Andersen, managing Director of BALS, says:
“We already have a lot of experience, but the energy price spikes have put further pressure on the need for change. Our 13 supermarkets have been modernized, and we have nearly no cost for heating in the stores because the heat comes from our freon-free refrigeration systems, solar cells, and heat pumps. It is an advantage with the current energy prices, and it reduces our CO2 emissions. We are proud to be part of one of the most energy-efficient supermarkets in the world and test the solutions that can help buildings become climate neutral.”
Why building a Danfoss Smart Store application development center?
In Danfoss Smart Store application development center in Nordborg Denmark we are integrating all the technologies relevant to the food retail sector, from natural refrigeration, energy efficiency, reducing waste and sourcing renewables - all in one installation.
ON DEMAND Smart store ADC webinar series

Smart Store learnings – Rail Heat Control - whitepaper
Read more about how supermarkets can achieve significant energy savings with proper rail heat control.
Scalable technologies
The installations and technologies in the supermarket are scalable. They can be applied in the smallest store up to the biggest hypermarket.
The supermarket cooling (refrigeration and comfort cooling) systems run exclusively on natural refrigerants (CO2). CO2-based refrigerants do not deplete the ozone layer and have the lowest possible Global Warming Potential (GWP) score. In addition, CO2 refrigerants outperform traditional HFC-systems when it comes to energy efficiency in different weather conditions.
The supermarket is equipped with a heat recovery unit capturing excess heat from the cooling systems to provide space heating for the entire store as well as the surrounding community through the district heating network. The heat recovery unit, can by re-using the excess heat from the cooling system, reduce the external heat requirement with up to 89,7%. Furthermore, the energy pack can supply additional heating and cooling when needed.
Smart energy systems applied
100 KW solar panels on the roof help to optimize store operations. On sunny days, solar energy can be accumulated in the freezers. Turning the temperature in the freezers further down from e.g., -18 to -25 help accumulate solar energy ( while reducing battery storage). When the solar panels are less efficient due to no sun the temperature rises back to normal settings.
Co-developing with customers
The supermarket has two separate refrigeration systems installed that run independently of each other. Therefore, operations of a supermarket continue while Danfoss co-develops new solutions with customers. And when future applications are being tested, the cooling cabinets and freezers stay cool.
Certifications
DGNB Silver (EU)
LEED Gold (USA)
The Smart Store provides inspiration for building DGBN / LEED certified supermarkets showcasing that it does not require a lot of extra resources to ensure that the building is healthy, future proof, and positively impacting the surrounding community.
Biodiversity
In order to positively impact the local biodiversity several initiatives have been taken. Very visible mega pergola surrounding the building which will be watered by use of collected rain- and surface-water. Also, different native grasses as well as a ‘green roof’ will be planted to create a micro-environment for biodiversity.
Cooling and heating capacity for 1,500 m2 store and 250 m2 ADC
30 kW medium temperature
13 kW freeze - low temperature
20 kW comfort cooling/ventilation for store and ADC (additional 20 kW from roof-top chiller)

Getting supermarkets to net zero
With the world’s population expected to reach 10 billion people by 2050, sustainable food retail and storage are more important than ever. Yet this is an often-overlooked step in the decarbonization of society.
Contact us
Want to experience real supermarket efficiency?
Reach out to us if you are interested in visiting our Smart store application development center and see it live.

New ‘Smart Store’ paves the way for 21st century supermarkets
New “Smart Store” will work as Danfoss’ test center for energy efficiency technology. ‘The Smart Store’ is expected to be approximately 50% more energy efficient compared to a typical supermarket with a first-generation CO2 refrigeration system.
Case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danish supermarket cuts heating bill and CO₂ footprint with Danfoss Heat Recovery Unit (HRU)A busy Danish supermarket reduced its annual heating bill by 89.7% and its CO₂ footprint by 6.7 tons a year by making use of the waste heat from its refrigeration system.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danish supermarkets turned into heat suppliersA Danish supermarket fulfills 95 percent of its heating demand from its own cooling display cases. The chain has installed Danfoss heat recovery units and managed to halve its CO2 footprint in five years. Imagine if this was done in all supermarkets in the world.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }They are the eyes and ears of DanfossDanfoss Enterprise Services in Baltimore delivers real-time insight to 14,000 supermarket operators and the demand is growing.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }A new shade of green for grocery storesThe supermarket aktiv & irma in Oldenburg, Germany, has pressed the start-button to a solution enabling it to store and generate electricity. The grocery store’s manager calls it a leap forward in energy supply. Danfoss and SMA have helped make it happen. Learn how.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }“A real win-win situation!” Danish organic food company reduces climate footprint with CO₂ cooling solutionA stronger environmental profile and energy savings of approx. 30% from a cooling solution that can be expanded as needed. These are the results so far for Danish organic food company Aarstiderne. Since Q1 2018, the company’s facilities at Barritskov, Denmark, have relied on a CO₂ cooling system with Danfoss components delivered by refrigeration installer company JF Køleteknik A/S.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }The Danfoss Multi Ejector range for CO₂ refrigeration: design, applications and benefitsDanfoss offers a complete portfolio of gas and liquid ejectors that provide significant benefits in CO2 refrigeration applications. Here we take a closer look at these offerings: the Multi Ejector Low Pressure (LP), the Multi Ejector High Pressure (HP), and the Liquid Ejector (LE). All three ejector products are only available as a complete Multi Ejector Solution™ where the ejector is bundled with the AK-PC 782A pack controller to provide the robust system controls necessary for efficient and reliable operation.
Related applications
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Case controlsYour refrigeration system is the natural place to look for energy efficiency gains. To unlock that potential, you need a controller, expansion valve, and high accuracy sensors that are smart enough to make the technology work together—and a system manager that can help you see and control the bigger picture.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }CO₂ in food retailDanfoss has pioneered CO₂ refrigeration systems for more than 10 years. Learn more about our CO₂ refrigeration solutions for supermarkets here.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Condition monitoring of HVAC/R systemsIn air flow and indoor air quality-related applications, condition monitoring functionality improves system uptime and competitiveness by preventing issues before they occur.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Emission monitoring for marineOur innovative sensors precisely and continuously measure climate parameters and environmentally harmful gases, providing documentation of regulatory compliance and essential input for energy optimization.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }HVAC integration in supermarketsAlign your heating, ventilation, air conditioning, and refrigeration systems, to save money, safeguard stock, and reduce your environmental impact. Integrated solutions unlock the full potential of each application and increases the efficiency of the entire system.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Monitoring and managementConnecting your refrigeration system to the cloud offers a world of possibilities to save money and improve food safety. Remote monitoring and management make it easy to check and triage system alarm.
Highlighted products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }CCMT electric regulating valves, transcritical CO₂The CCMT is a highly reliable electric pressure regulating valve optimized for transcritical CO₂ refrigeration. The valve has versatile applications in the transcritical system.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }System managersThe system manager is the key component of the intelligent Danfoss ADAP-KOOL® refrigeration system for food retail.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Pack controllersDanfoss offers a range of compressor and condenser capacity controls for use in food retail, in compact systems as well as in large power packs.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Programmable controllers - MCXDanfoss’ range of universal MCX programmable controllers offers the functionality and reliability you need to get the best out of your heating, ventilation, air-conditioning and refrigeration (HVAC/R) equipment.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Solenoid valves for high-pressure CO₂ cooling applications in Food RetailEVT high pressure range is a direct or servo operated valve specially designed for CO2 transcritical refrigeration systems.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Multi Ejector Solution™The Danfoss Multi Ejector Solution™ ensures that transcritical CO₂ applications for retailers become energy efficient in any climate.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Evaporator and room controlDanfoss offers a range of evaporator controls with thermostatic expansion valves or with electric expansion valves.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }HRU - Heat Recovery UnitThe Danfoss Heat Recovery Unit helps to eliminate the technical challenges of managing heat recovery.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }AKV electric expansion valvesFor robust, efficient, and responsive control, Danfoss world-renowned, ADAP Kool® expansion valves, AKV, cover applications ranging from lower capacity commercial applications with CO2 and HFC refrigerant to large industrial applications with ammonia as a refrigerant.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Temperature sensors for coolingRefrigeration temperature sensors are used for applications within air-conditioning as well as commercial and industrial refrigeration applications. The Pt 1000 sensor element meets the DIN/IES 751 class B requirements and ensures an accurate and reliable temperature signal applicable for regulation, safety, and data logging.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Air Conditioning & Refrigeration Pressure TransmittersRefrigeration pressure transmitters are used for commercial air-conditioning and for commercial and industrial refrigeration applications. They are made in stainless steel to be compatible with fluorinated and natural refrigerants and laser welding with no soft seals ensure hermetic tightness for decades.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® HVAC Drive FC 102This tough and savvy FC102 drive enhances pump and fan applications in building management systems, and runs outdoors in most climates.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }VLT® Refrigeration Drive FC 103FC 103 is dedicated to controlling compressors, pumps and fans for significant energy savings in refrigeration plants.