With Danfoss systems you never need to worry about legionella or insufficient or cold water in the bathrooms. Our domestic hot water solutions include water heaters that can be connected to multiple tanks as well as storage and charge systems, hot water valves that prevent legionella, temperature controllers and self-limiting heating cables that are used for temperature maintenance. When used together, these combine the demand for high performance, comfort, hygiene and resource efficient operation – even during peak loads.

Production of hot water
Production of hot water is done by one of our water heaters. These can be equipped with one or more storage tanks to provide enough hot water at peak loads. They can also be equipped with a storage charging principle. They meet hygienic, safety and temperature requirements and can be connected to different energy sources. Adding hot water valves and temperature controllers help prevent legionella. All together a high performance, comfortable, hygienic and resource efficient production of DHW is achieved.

Distribution of hot water
The hot water is then distributed to the water tap points. In most cases the size of the building requires a series of risers circulating the hot water. Our Thermal balancing valves ensure the proper hydronic balance that avoids long waiting times. As these control the water temperature they also avoid too hot water causing lime, corrosion and energy inefficiency. Normally these valves are set to a temperature that avoids legionella to grow.

Smart and energy efficient legionella risk reduction
The thermal balancing valves can be equipped with thermostatic or electronic disinfection modules, allowing periodic flushing of the system to kill the legionella bacteria. The electronic temperature registration system monitors all the temperatures and initiates the safe and energy efficient disinfection cycle. It also stores the temperature data for logging purposes. The electronic controller can be easy accessed on mobile devices using Wi-Fi or be integrated into Building Management Systems (BMS) for remote control, monitoring and alarm purposes.
Close to the water tap points, there is sometimes a need to lower the hot water temperature. Our hot water mixing valves ensure the outlet water temperature is safe for consumption.
Healthy Solution
Self-limiting heating cables provide power only where needed adapting output according to the ambient temperature. It helps to reduce water waste as you can get hot water immediately providing appropriate disinfection to suppress the Legionella bacteria.

How to balance domestic hot water systems?
What are the issues and challenges in domestic hot water systems in non-residential buildings?See why hydronic balancing is important, what type of balancing is the best and how that can solve the issues.
How we can help you
One partner with high DHW expertise
High performance and energy efficiency
Comfort
Hygiene
Resource efficient operation
Reduced risk of legionella contamination
Lowest possible operating costs

MTCV Thermal balancing valves with CCR2+ electronic controller
Establish safe and energy efficient DHW systems and control them remotely on a mobile device.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Rotary valvesRotary valves are primarily designed for regulation of flow and temperature in heating systems where a certain leakage can be accepted and where a defined control characteristic is not required.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }SubstationsSubstations are house heating systems or units in apartments that handle heat transfer from district heating pipes into your home to get hot water and heat on demand.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Domestic hot water systems with tankThe water heaters with tank are suitable solutions for hospitals, sports arenas, hotels, apartment blocks and similar large buildings. The product range covers storage and charge systems which all combine the demand for high performance, comfort, hygiene and resource efficient operation.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }MTCV with CCR2+MTCV Thermal balancing valves provide a dynamic, temperature based, balancing solution for drinking water applications. Combined with the CCR2+ a smart and energy-efficient electronic control solution for monitoring and disinfecting DHW systems is established.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Self-acting temperature controllersThermostatic temperature controllers are used to control the flow temperature in instantaneous/storage domestic hot water and heating systems. In multi-family houses and commercial buildings, they are used for hot water systems and for return temperature limitation in district heating applications.
Articles
Coming soon...
Coming soon...
News
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Introducing the Next-Generation AME 110NL(X) Modulating ActuatorsWednesday, September 25, 2024The 2nd generation of AME 110NL(X) actuators for AB-QM 4.0 valves are significantly upgraded and designed to enhance the performance and efficiency of hydronic HVAC systems. These advanced actuators replace the existing AME 110NL(X) and AME 120NL models and deliver high-precision control due to the built-in digital step motor which has a 15x higher resolution as its predecessors.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Expanding the AB-QM family with AB-QM 4.0 CO6 FlexoThursday, July 25, 2024AB-QM 4.0 CO6 Flexo, is a standardized prefab PICV connection set especially developed to streamline the design, installation, and servicing of hydronic HVAC systems, specifically radiant panels and chilled beams in four-pipe heating and cooling change-over systems.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Legionella prevention, the smart wayMonday, September 24, 2018For many years Danfoss has played an important role to establish safe Domestic Hot Water systems in hospitals, hotels, multi-family apartments and other buildings. Now our MTCV thermal balancing valves and new CCR2+ electronic controller for automatic disinfection have been significantly improved to your benefit.