• My Apps
    My Apps You will have the option to use My apps once you login.

What is SiC power module?

silicon carbide power module

SiC power modules

Danfoss offers a wide range of innovative custom-made SiC power module solutions for industrial, e-mobility and energy applications.

Today, the most widely used material for power semiconductors is silicon. Silicon is inexpensive to produce and the technology is well understood. However, there are other materials, the so called compound power semiconductors, such as Silicon Carbide and gallium-nitride that are much more efficient conductors of electricity. This means that less energy is lost through heat in any power conversion process which has the added benefit of reducing the need to have expensive cooling systems as well as lowering the size and weight of the power electronics unit.

Learn more about what Silicon Carbide power modules are, how they work and why SiC is preferred in selected applications.

Did you know?

To facilitate the growing demand for Silicon Carbide (SiC) power modules worldwide, Danfoss has established a “SiC Center of Excellence” in Munich, Germany containing offices and a 600m² lab. Besides qualification and development of semiconductors and different test scenarios, the new lab is also qualified and equipped for high power tests up to 400kW.

The purpose of the Danfoss’ SiC Excellence center is to support in the development of customized power modules and power stacks in a variety of customer projects, requiring SiC power modules. In addition, the SiC-team is also researching on future power module generations, including the fast switching SiC-semiconductors and their switching behavior.