Digitalization

  • if (isSmallPicture) { MyDrive Suite featured on a desktop, laptop, tablet, and mobile; } else if (isBigColumns) { MyDrive Suite featured on a desktop, laptop, tablet, and mobile } else { MyDrive Suite featured on a desktop, laptop, tablet, and mobile }
    Ever thought about how software has transformed the journey from design to commissioning of a drive?

    In recent years, software evolution has completely revolutionized the way we work with drives, right from the design stage, through to commissioning and operation. Now we've released MyDrive Suite, a software hub where all Danfoss Drives software tools are centrally located.

  • if (isSmallPicture) { Infographic showing data center energy distribution; } else if (isBigColumns) { Infographic showing data center energy distribution } else { Infographic showing data center energy distribution }
    Where does data center CSR intersect reduced carbon footprint?

    Data centers can reduce their impact to the point of climate neutrality in three ways, all without compromising data availability: lowering power usage effectiveness (PUE), integrating renewables and storage into data centers, and using waste heat from data centers for heating and/or desalination.

  • if (isSmallPicture) { Water leakage on a city street; } else if (isBigColumns) { Water leakage on a city street } else { Water leakage on a city street }
    The hidden solutions for limiting water scarcity

    It’s estimated that more than 30% of all the global clean water produced for household use/cities is lost in leakage. Often digitalization and VSDs are the key components to help limit water scarcity issues instead of creating new water facilities.

  • if (isSmallPicture) { Nordhavn, Copenhagen in Denmark. ; } else if (isBigColumns) { Nordhavn, Copenhagen in Denmark. } else { Nordhavn, Copenhagen in Denmark. }
    To enable Europe’s clean energy future, we need to buckle up and couple up

    The theme for this year’s EU Sustainable Energy Week is ’Shaping Europe’s Energy Future’ – that future holds plenty of potential and must rest on further integration across sector and policies to ensure we optimize our energy systems for optimal performance and efficiency.

  • if (isSmallPicture) { Infographic about hybridization; } else if (isBigColumns) { Infographic about hybridization } else { Infographic about hybridization }
    Disrupting the electricity system

    The three trends of decentralization, digitalization and electrification have the potential to disrupt the conventional electricity system, and they reinforce each other in a virtuous cycle.

  • if (isSmallPicture) { VLT AutomationDrive FC 302; } else if (isBigColumns) { VLT AutomationDrive FC 302 } else { VLT AutomationDrive FC 302 }
    The versatile, reliable and consistently awesome AC drive

    It may have been around for a while. But that doesn’t mean it hasn’t evolved. Far from it. The VLT® AutomationDrive FC 300 Series is now tougher and more intelligent than it has ever been before.

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Ready-made energy solutions #9 and #10

    We have to exploit the potential of digital, connected solutions. Smart control of heating, cooling and ventilation can double the performance of these technologies. On average, energy consumption can be reduced by 38% per building.

  • if (isSmallPicture) { Ready made energy efficiency solutions; } else if (isBigColumns) { Ready made energy efficiency solutions } else { Ready made energy efficiency solutions }
    10 ready-made energy-efficiency solutions

    In a series of posts we present 10 ready-made solutions for more energy efficiency. We’ll discuss how it’s important to get the basics right and how taking a system approach is the way to go. We’ll talk about energy recovery and sector coupling. And, finally, well explain why it’s essential to exploit the potential of digitalization to create new business models and optimize processes.

  • if (isSmallPicture) { Danfoss local control panels (LCPs); } else if (isBigColumns) { Danfoss local control panels (LCPs) } else { Danfoss local control panels (LCPs) }
    Customers feel the need – the need for speed!

    How can a large company, such as Danfoss, respond to specific market requests in months instead of years? The answer, as you’ll find out by the example in this post, lies in a perfect convergence of close customer interaction, digital design, 3D printing and an iterative approach to development.