When we talk about sustainability, much of the conversation is centered around resources. Water, oil, gas, iron — these raw materials are either central to our current problems, our future solutions, or both.
There is, however, one raw material above all others. Data. Because we can’t manage what we don’t measure — and, at Danfoss Digital Services, we make data work for you.

Harness the power of digitalization
At Danfoss Digital Services, we are developing cutting-edge technology that accelerates the green transition. Our datadriven approach is optimizing energy use, eliminating food waste, and reducing carbon emissions — and we’re not stopping there. Data and connectivity can deliver the key emission reductions that we need. We are ready to help you decarbonize tomorrow.
Sustainability through digital innovation
Danfoss Digital Services is a dedicated business unit of software development specialists committed to sustainable solutions through digital innovation. Our approach is based on the existing expertise earned from our foundation solutions — Alsense and Leanheat.
Both solutions analyze data to provide real-time insights and genuine efficiency for our customers.

Alsense® Food Retail Services — Less Waste. More Sense.
One third of all food produced today is lost or wasted. In fact, if food waste and loss was a country, it would be the third largest greenhouse gas-emitting country in the world (UN FAO).
Alsense helps eliminate food waste and optimizes cooling efficiency for supermarkets and food retailers through intelligent data.
Alsense® customers




Leanheat® — For true energy optimization. From people to production.
Buildings account for a staggering 40 percent of the world’s energy consumption. And in Europe alone, almost a third of residential heating comes from fossil fuels.
Leanheat empowers district energy networks to optimize the operational efficiency of buildings and increase the comfort of end-users through end-to-end software solutions.
Leanheat® customers




Talk to an expert today
At Danfoss Digital Solutions, we make data dance. We love nothing more than crunching numbers and creating bespoke solutions to accelerate the green transition.
Achieving energy and resource optimization isn’t a solo project. It takes true collaboration, so if you have a problem that you think we could solve, please book a meeting with one of our experts today.
Case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Roll-out in 50,000 housing units: enercity AG optimizes district heating supply with Leanheat® BuildingThe AI-powered software Leanheat® Building helped Hanover’s district heating utility systematically integrate the buildings side of the network and achieve a 5-10% reduction in energy consumption and a 20% reduction in peak loads.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Flue gas heat recovery to enhance sustainable heating for Frederikshavn residentsFrederikshavn DHU operates a 14-megawatt gas boiler to provide essential heating services during colder periods. To improve energy efficiency and reduce environmental impact, a project was initiated to recover more energy from the flue gas emitted by the existing biomass boiler system.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Apartment block saves energy and money with AI and dynamic balancingCentrally heated apartment buildings often suffer from variations in room temperatures due to inefficient and unbalanced heating systems. This can lead to unhappy residents complaining about lack of comfort or high energy bills. Swedish cooperative organization HSB aimed to use an intelligent monitoring and control solution to improve the energy efficiency and indoor comfort of a 12-apartment block that is connected to district heating.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danfoss’ Leanheat® Building helps Avain deliver energy-efficient heating to residents throughout FinlandAvain has installed Danfoss' modern SCADA solution, Leanheat® Building in over 100 new and renovated residential properties containing nearly 3,000 apartments.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Leanheat® Building helps City of Espoo save 200,000 EUR in energy costsWhat can be achieved when a large energy company, a city that has set itself tough sustainability targets and a pioneer of digital solutions for energy efficiency all sit around the same table?
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Optimizing the efficiency of district heating system in Altensteig, GermanyStadtwerke Altensteig (Baden-Wuerttemberg) is one of the first district heating network operators to use the brand new Leanheat® Monitor software that offers operators a complete package for the operation of their district heating network.
Meet our people





Are you also a digital superhero?
Do riddles and puzzles get you out of bed in the morning? Do you eat data for breakfast and reorganize your house on weekends in search of ultimate efficiency? If you’re nodding to yourself, you just might be our next colleague at Danfoss Digital Services. Here, we build digital solutions that count — crunching data to help accelerate our customers’ green transition. Are you our next digital superhero? Whether you are an experienced professional or just starting out, we have a cape that fits.
Events
Coming soon...
Coming soon...
News
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }HOFOR and Danfoss future-proof heating in Copenhagen with a new data solutionFriday, December 6, 2024Danfoss and HOFOR are ready to optimize Copenhagen's future district heating with AI technology.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danfoss completes acquisition of ENFOR’s district energy efficiency softwareTuesday, January 2, 2024Danfoss A/S has acquired ENFOR’s district energy software business, with plans to scale its advanced AI driven energy efficiency optimization worldwide, to enable the decarbonization of cities.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Danfoss and HOFOR partner to maximize building energy efficiency with AI powered Leanheat® Solution.Monday, November 20, 2023Two Danish powerhouses partner to continue strategic collaboration to enhance energy efficiency and reduce overall energy consumption in multifamily buildings.
Contact us
Partner with us

Partner with us
At Danfoss, we truly believe that the green transition will only be possible with genuine collaboration. Our Digital Services partners cover a wide range of industries and locations to ensure support for our customers where and when they need it, as well as broaden the reach and impact of our solutions.
We are always on the lookout for potential new partners in the following fields:
Technology — Help us build our next great solution at Danfoss Digital Services.
Potential partners: OEMs, independent software vendors
Knowledge — Help us innovate and investigate the latest technologies.
Potential partners: Universities, research institutions, industry groups
Commercial — Help us get our solutions to those who need them.
Potential partners: Digital wholesalers, software distributors
Service — Help us meet our customers’ needs — wherever, whenever.
Potential partners: Systems integrators, remote service providers, business consultants