Danfoss helps set new world record in SWRO energy efficiency

Thursday, June 20, 2024

When Spain’s Canary Islands Institute of Technology (ITC) announced a new world record for SWRO energy efficiency this May, Danfoss high-pressure pumps were at the heart of the innovative solution. The breakthrough could have significant consequences for a thirsty world facing the combined threats of water scarcity and climate change.

Desalination is an increasingly critical source of drinking water for millions of people worldwide. But while seawater is abundant and “free of charge,” the electrical energy required by the seawater reverse osmosis (SWRO) process that drives most plants comes at financial and environmental costs. Now, researchers in Spain have shown the way to record-breaking SWRO energy efficiency – all made possible by Danfoss APP high-pressure pumps.

DESAL+ LIVING LAB is a public-private ecosystem for innovation in seawater desalination located in the Canary Islands. ITC initiated the DESALRO 2.0 project to reduce the specific energy consumption (SEC) of an SWRO plant to below 2.0 kWh/m3. UTE Canaragua-Elmasa was in charge of the plant execution. 

With the previous world record of 2.27 kWh/m3, set in 2021 in Saudi Arabia, this 12% reduction in total energy usage per liter of drinking water would be a significant achievement. In the end, the DESALRO 2.0 project not only broke through the 2.0 barrier but went even further by establishing the latest standard of SWRO energy efficiency at 1.861kWh/m3 – a full 18% lower than the previous world record.

Positive displacement high-pressure pumps made by Danfoss make it all possible

In line with the pre-design criteria established by the Canary Islands Institute of Technology (ITC), the DESALRO 2.0 project utilized the most energy-efficient pump type available to create the plant’s high pressure: positive displacement pumps. This is a crucial criterion since high-pressure pumps typically consume about 70% of an SWRO plant’s energy.

Accordingly, Danfoss APP pumps, which are positive displacement pumps utilizing an axial piston design specifically engineered for reliable energy efficiency, supplied all the high pressure for the record-setting plant. For more information on the energy efficiency advantages of positive displacement pumps, please see this article from Pumps & Systems.

The DESALRO 2.0 breakthrough could have important consequences for a thirsty world that also needs to decarbonize

The success of DESALRO 2.0 marks a critical step forward in making SWRO more energy efficient.

New SWRO plants operating at this efficiency would be less expensive to operate and have a lower carbon footprint than what is now common, thus making this source of fresh water more available to some of the growing number of people facing water scarcity. At the same time, retrofitting existing desalination plants to be as energy efficient as is now technologically possible would result in significant savings on electricity costs and GHG emissions.

Retrofitting existing plants to be more energy efficient: An essential strategy for SWRO decarbonization

As we discussed in a previous blog, the quest for energy efficiency is a key driver in the evolution of the desalination industry.

Historically, the first desalination plants using thermal distillation had SECs of up to 27 kWh/m³, roughly 1400% higher than the new world record. Subsequent generations of SWRO plants have evolved to be far more energy efficient. However, most existing SWRO plants still have significantly higher SECs, often ranging from 2.5 to 3.5 kWh/m³ and even higher.

According to calculations in our blog, if all existing desalination plants worldwide were retrofitted to operate at 2.0 kWh/m³, the potential global savings would be enormous:  

  • Energy savings: 247 TWh, equivalent to Spain’s total electricity usage in 2020
  • Financial savings: €34.5 billion, enough to build seven wind farms the size of Hornsea Project 1
  • Carbon emissions savings: 111 million metric tons of CO₂, surpassing the annual emissions of Bangladesh

With potential energy savings of this magnitude, it is reasonable to hope that more SWRO decision makers will be inspired by the new world record to critically examine the energy efficiency of their current and upcoming plants.

Innovation and scalability are key to reaching global decarbonization goals

According to Danfoss HPP’s director of innovation, Georg Herborg, the Spanish achievement is an inspiration for the entire SWRO industry. “The new world record is a major milestone that should be celebrated,” he says, “but there is still plenty of work to make SWRO and other high-pressure membrane processes even more energy efficient. Our R&D team is working on these challenges together with industry partners every day.”

Georg Herborg, Director of Innovation

“The DESALRO 2.0 project is a great example of a public-private enterprise cooperating with university researchers to make a real impact. Of course, we’re honored that they specified Danfoss high-pressure pumps for this breakthrough, but we’re also excited about how they set up the project.”

Georg Herborg, Director of Innovation

“For one thing, the world-record project uses existing, off-the-shelf technology – components that anyone can source today. For another, the ITC has emphasized the importance of the replicability and scalability of this record-breaking project by indicating that the same positive displacement pump technology, with efficiency above 88%, must also be able to drive trains between 5,000 -10,000 m3/day. Danfoss APP pumps that deliver this capacity with efficiencies above 90% are available now, and our R&D team continues its work to improve this even more. We look forward to the next records the innovative people of the Canary Islands will set, and we will do our part to be part of the solution!”

For more information on the DESALRO 2.0 project (in Spanish), watch this video produced by the Canary Islands Institute of Technology (ITC).

About the Canary Islands Institute of Technology (ITC)

 

 

The Canary Islands Institute of Technology (ITC) is a research and development organization based in the Canary Islands, Spain. Established over 25 years ago to foster innovation and technological advancement, the ITC focuses on renewable energy, water management, and sustainable development. The institute collaborates with various industries, academic institutions, and government bodies to drive scientific research, support economic growth, and address environmental challenges.

For more information, please visit https://www.itccanarias.org

About DESAL + LIVING LAB

 

 

 

DESAL+ LIVING LAB is an innovative research and development platform dedicated to desalination and water treatment technologies. Located in the Canary Islands, the public-private ecosystem serves as a collaborative hub where scientists, engineers, and industry experts work together to develop and test advanced desalination solutions. DESAL+ LIVING LAB focuses on improving the efficiency, sustainability, and cost-effectiveness of desalination processes, aiming to address global water scarcity challenges. 

For more information, please visit https://www.desalinationlab.com

About Elmasa

 

 

With more than 50 years of existence, Elmasa is a specialist in the management of water treatment projects. Management that covers all possible areas, from the design to the construction phase, to the service start up and operations and maintenance. The environment is taken care of throughout the whole process as sustainability is a high priority for the company.

For more information, please visit http://www.elmasa.es/en 

About CANARAGUA

 

 

Canaragua provides a comprehensive array of water management services to households, businesses and municipalities throughout the Canary Islands and beyond. With its dedication to harnessing technological innovation to serve its customers while protecting the environment, Canaragua leads the way throughout the water management cycle, from catchment to drinking water treatment, transportation and distribution, sewage infrastructure, and wastewater treatment.

For more information, please visit http://www.canaragua.es/en 

Read more about APP pumps