Norway’s leading producer of sustainable salmon unveils first hybrid fish farming boat
- Edel is the first hybrid vessel built for the aquaculture sector by Norwegian shipyard Moen Marin. It is NRS Farming’s first diesel-electric boat.
- Danfoss Editron has supplied two 105kW permanent magnet motors which will drive the vessel’s propellers.
- NRS Farming intends to run the vessel solely on battery power during short trips. When working on fish farming sites, it will operate in diesel-electric mode on longer journeys.
TRONDHEIM, NORWAY – Danfoss Editron has delivered two 105kW motors that will help power Edel. This is the first hybrid vessel built for the aquaculture sector by Norwegian shipyard Moen Marin. Edel is also the first diesel-electric vessel in the fleet of NRS Farming, Norway’s leading producer of sustainable salmon.
The 13.5 by 7.5m vessel will become part of NRS Farming’s fleet. It will be used for sustainable fishing in salmon farms located in Norway’s fjords. As it has an operating pattern of predominantly short trips, NRS Farming plans to run Edel mainly on battery power. However, the boat will operate in diesel-electric mode on longer journeys, with the battery pack charged by the diesel generator.
Danfoss Editron’s motors operate on synchronous reluctance assisted permanent magnet (SRPM) technology. These are liquid-cooled and designed to work in harsh operating environments such as the marine sector. As well as the motors, Edel also features 10 sets of lithium-ion batteries with a total capacity of 244kWh. Moreover, two electric capstans, a 139kW generator, a 50hp thruster and a fully-rotating deck crane.
Ole Duus, Sales Area Manager for Danfoss Editron, said:
“Compared to conventional technologies, such as induction machines or standard permanent magnet motors, our electric SRPM motors are smaller, lighter in weight and offer higher efficiencies. These are key factors as to why more and more customers in the marine sector are choosing to work with us to electrify their ships.”
Arve Olav Lervåg, Executive Vice President of NRS Farming, added:
“There are many clear advantages of going for a hybrid vessel, both in terms of climate and environmental benefits and reduced diesel costs. But the most important thing has always been to look after our employees. We get a better working environment with less noise, exhaust and vibrations.”
![Danfoss Editron](/media/11917/dps_editron_boat.jpg?anchor=center&mode=crop&width=810)
Danfoss Editron
Danfoss Editron is taking fuel savings and energy efficiency to the next level. We specialize in hybrid and electric powertrain systems for marine, off-highway and commercial transport markets. Our mission is to end pollution through electrification.