Danfoss Power Solutions extends its PLUS+1® Partner Program with two new partners
HMI Systems and PRECO Electronics have joined LINAK as members of Danfoss Power Solutions’ PLUS+1® Partner Program. The move will enable customers to simply and quickly incorporate complementary non-Danfoss hardware components with electrical interfaces into their mobile machines utilizing PLUS+1® GUIDE and PLUS+1® Service Tool.
HMI Systems now offers PLUS+1®-compliant keypads for off-highway vehicles. Together with Danfoss Power Solution’s range of displays, joysticks and HMR CAN Rotary devices, customers can easily design a modern cabin interior. They can also use the PLUS+1® Service Tool to create customized service applications for easy machine tuning, diagnostics and troubleshooting.
PRECO Electronics offers autonomy, object detection and collision mitigation solutions through its radar platform that can be integrated into heavy-duty equipment. Safety around machines can be challenging, with low visibility in some directions due to blind spots from the driver’s seat of the vehicle. Using Danfoss Power Solutions’ PLUS+1® GUIDE advanced mobile machine control will speed up the implementation of the radar on a machine by quickly decoding data into tangible information.
Commenting on the additions of HMI Systems and PRECO Electronics to the PLUS+1® Partner Program, Danfoss Power Solutions’ Digital Platforms Program Director Thomas Palmgren said:
“We’re looking forward to our new PLUS+1 Platform Partners contribution to our PLUS+1 family, as enabling more PLUS+1®-compliant products provides a host of benefits to our PLUS+1 programming community."
Through our PLUS+1® Partner Program, we want to be able to offer a broader portfolio to our customers from which they can build their machines. While we don’t have the opportunity to manufacture all of the products ourselves, customers can easily integrate Danfoss PLUS+1®-compliant products from our partners, which makes integration faster, easier and safer.”
Davis Hague, OEM Business Development Manager - Off Road at PRECO Electronics added:
“Danfoss Power Solutions is a leader in system integration and control, with the company’s PLUS+1® platform providing end-users with seamless integration capability. As technology advances, our radar must readily integrate with sensor fusion and machine functionality. The combination of our radar with Danfoss Power Solutions’ PLUS+1® platform will deliver seamless integration to end-users across the globe.”
![PLUS+1® Partner Program](/media/xolpf2ku/plus-1-partner-program-slider.jpg?anchor=center&mode=crop&width=810)
PLUS+1® Partner Program
Our PLUS+1® Partner Program consists of a select group of companies with complementary products which integrate into PLUS+1® systems the same way all Danfoss hardware components do.