Easy snow, ice and frost removal with DEVI by Danfoss
From homes and offices to castles and stadiums, DEVI electric heating products have been installed on commercial and residential buildings and areas around the world as an effective solution to remove snow and ice.
DEVI electric heating systems consist of three main components:
- a heating element (cable or mat with suitable specific output)
- a controller (with air and humidity sensor)
- and additional accessories depending on the selected equipment (e.g. clips, fixing tapes, or others).
Flexible heating elements for outdoor areas
The heating elements are extremely versatile, as they can be installed on almost any type of building construction, and can be placed wherever they are needed, to prevent the buildup of snow.
For example, installing DEVI electric heating under a concrete layer on steps, pavements, driveways, paths, etc., will ensure that snow melts and drains away. These areas then remain dry and safe to walk on, helping to reduce the risk of trips and falls. When applied to a roof, electric heating melts ice to stop hazardous icicles from forming around gutters.
The heating system works automatically 24/7, which helps protect the building from potential damage caused by frost, snow and ice throughout the winter months. It also reduces the amount of time and money spent on manual labor required to shovel snow, lay grit or salt, and remove ice.
![](/media/qh1lbvel/outdoor-safety-commercial-1920x420.jpg?width=420&height=1920&rnd=133189365029130000?anchor=center&mode=crop&width=1920&height=420)
Frost and Snow protection of commercial areas
Utilize energy-efficient technologies to address seasonal challenges, and use electric heating mats or cables to protect commercial spaces from snow, ice, and frost damage.
Future-proof and energy efficient
Chemicals are often used for de-icing, but these run off into soil and surfaces causing damage to plants and the environment. These days, planning winter protection for urban spaces and renovations requires different solutions that are long-lasting and sustainable. DEVI electric heating systems come with a 20-year warranty and are maintenance free, contributing to a lower total running cost.
Importantly, electric heating is energy efficient as it uses low amounts of electricity, without compromising output or performance. The global trend towards the use of electricity as a renewable energy source means electric heating is ideally positioned as a future-proof solution for snow and ice removal.
80 yrs of experience and product innovation
For 80 years our solutions for outdoor safety and indoor comfort have been improving people’s quality of living. They were installed in thousands around the globe. Click here to discover how DEVI snow and ice melting systems have been used to protect buildings and maximize safety in public areas facing harsh winter conditions.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Heating CablesOutdoor heating cables are used for efficient snow removal and ice prevention. They provide safety for people, buildings, and the environment. It is a sustainable solution for a green and clean future through low energy consumption during the frost period.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Self-limiting cablesSelf-limiting heating cables are designed with a temperature-dependent resistant element between two parallel copper bus wires. When the bus wires are connected to the mains, a current goes through the temperature-dependent resistant element which will then heat.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Analogue controllersAnalogue controllers are thermostats with temperature sensors allowing you to switch the system on and off depending on settings.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Digital controllersDigital controllers have unique features allowing you to reduce energy waste. Equipped with temperature and moisture sensors, control modes, and special functions, they ensure accurate temperature settings, reducing energy consumption costs by up to 40 percent.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Heating MatsThe outdoor heating mats are designed for melting ice and snow and may be installed into special mastic for ground, grass and asphalt constructions. Mats are available in different lengths for two power supply options—230 and 400 V.
Related application
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Electric heating frost and snow protection system used in application in pavementIce and snow melting systems are used in various applications in parking lots, garages, stairs, pavements, and other ground-level surfaces. They secure personal safety in hazardous winter conditions. Our systems can be installed on roofs, in gutters, pavements, and many more areas in and around the house. There is a wide range of products available such as cables or heating mats, specialized controllers, and mounting accessories. And you can count on us for knowledgeable support and service.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Frost and snow protectionDuring winter time it can be hazardous to access commercial or public buildings. Snow covered parking lots, garage ramps, stairs and pavements need to be cleaned to allow visitors safe access. Danfoss offers highly effective frost and snow protection systems including all necessary products such as electric heating cables or mats, controllers, sensors and mounting accessories.
Related case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Electric heating systems for the conservation of old castlesThe Örebro Castle is a medieval castle fortification situated in the scenic region of Närke, Sweden. The castle lies on an island by the river Svartån. The oldest part of the castle, a defense tower, was erected in the latter half of the 13th century, but its present appearance, the Örebro Castle, was constructed over the last century. Since 1935, the castle has been a national Swedish monument.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Electric heating system to prevent the condensation in the Woolworths Distribution CentreThe Woolworths Distribution Centre was experiencing condensation due to the temperature differences between the cold storage facility and their offices. This resulted in water dripping hazards in the meeting rooms, canteen, and offices.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }The Bjørvika Tunnel, Oslo, NorwayElectric heating for the immersed tunnel in Norway.
The Bjørvika Tunnel is a motorway immersed on European Route E18 in the city center of Oslo. The tunnel links Festning tunnel in Oslo west with Ekeberg tunnel in Oslo east. The completed tunnel has an unbroken length of six kilometers. The Bjørvika Tunnel is the first immersed tunnel in Norway.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Electric heating ensures safety along the asphalt driveway, Ankara, TurkeyProtocol Road, the longest asphalt driveway equipped with electric heating, is located in North Ankara, Turkey. The electric heating was installed along this 3.3 km 2-direction (3 lanes each) road connecting Ankara city center and the airport.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Electric heating chosen to protect 18th-century baroque palace in KyivDesigned by Bartolomeo Rastrelli in the second half of the 18th-century, Mariinskyi Palace is the official ceremonial residence of the President of Ukraine and used for hosting other heads of state. Electric heating was chosen as a sustainable modern technology to protect the historical landmark during its reconstruction.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }An ideal field is an integral part of a successful gameFor professional and international stadiums, a very high standard of playing surface is required. It is important to eliminate the risk of match cancellations, particularly those associated with poor weather conditions e.g. heavy rainfall or ice and snow.