![](/media/ivnlqmtf/cbm-mct10-1120x747.jpg?anchor=center&mode=crop&width=520)
Danfoss’ VLT® Motion Control Tool MCT 10, an interactive software used to quickly and easily configure and document the settings of AC drives, is now updated. Enjoy the support of additional sensors and the monitoring of permanent magnet motors in your CBM setup with the latest drives firmware.
If you are utilizing condition-based monitoring (CBM) in your AC drives already, you can now make fully use of the CBM functions via your computer.
With VLT® Motion Control Tool MCT 10 software version 5.21, you can monitor your entire system more effectively and reduce commission time to allow for easier monitoring, faster diagnosis, improved troubleshooting (alarms/warnings) and better preventive maintenance.
Save time on commissioning through guided step-by-step setup and fast verification of settings and functionality. A control panel simulator has been integrated for the VLT® series of drives so you can easily try out the programming of the drive in the software tool and follow the individual steps.
A major addition is the multiple drive handling which makes it possible to copy drive settings easily from a master setting to a large network of connected drives saving time and cost. The user-friendliness of the software has also been revised and adapted to that of the LCP operating panel. Improved graphical parameters allow for easier interpretation of data and guidance through the setup. A graphical overview of the limits and actual state allow for clearer monitoring and better troubleshooting of system analysis. For example, active parameters can now be highlighted in color to visibly distinguish them from inactive parameters. This makes commissioning with the tool clearer, easier, and faster.