Product milestone – 50 years of efficiency in operation

Wednesday, September 4, 2024

For 50 years, Danfoss’ reliable sensors have helped supertankers secure efficiency in operation and optimization of the energy output.
Supertankers sailing the world seas are built to withstand harsh conditions from the humid southern hemisphere to the heavy, cold storms on the North Sea. But it’s what’s inside, that matters. Behind the long vessel’s hull, Danfoss’ Sensing Solutions are working hard to reduce energy costs, monitor engine operations, and convert power optimally.

This year marks the 50-year anniversary of the first Danfoss pressure transmitter - the EMP - introduced to the market. The pressure transmitter monitors and controls in marine and industrial applications.

Thomas Schaukal, Sales Director, Danfoss Marine with nearly 30 years of experience in the business says:

“Our EMP2 pressure transmitter has stood the test of time and remains a popular choice among customers. The reason it is still a popular choice is the reliability, and our design fits on the engine applications. It is small, but an important part of a whole system.”
                                                                               -

The housing is still the same as when it was introduced to the market however, the sensor inside has undergone changes throughout the years. Today, the signaling is handled by a small built-in computer which means the sensor can be programmed for more functions.

Since the introduction of the first sensor, Danfoss has expanded the portfolio to include a wide range of robust sensors for various applications, including engines, gears, exhaust systems, and compressors.
Helping the marine industry decarbonize
Originally designed for marine and industrial applications, the EMP pressure transmitter offers a reliable pressure measurement, even under harsh environmental conditions.

Globally, more than 100,000 commercial and 25,000 naval vessels operate and over 90% of world trade is carried by sea. According to the international maritime organization, IMO, the maritime industry has set targets to reach climate neutrality by 2050.

Danfoss sensors will continue to be essential in marine applications reducing energy costs and emissions. And the number of sensors on each vessel keeps growing as data output has become key.

The high accuracy pressure transmitter EMP2 is designed for monitoring and control in marine and industrial applications and offers a reliable pressure measurement, even under harsh environmental conditions.

Bert Labot, Vice President, Danfoss Sensing Solutions says:

“We see a strong trend in the market towards capturing more data in all types of applications such as pumps, motors, and chillers. This will continue. With the decarbonization of the marine industry and vessel owners taking more alternative fuels into use the demand for sensors and continuous monitoring and prediction of maintenance keep growing. We will have the right product offerings to our customers.”

  • if (isSmallPicture) { Box type marine approved pressure transmitter type EMP 2 danfoss; } else if (isBigColumns) { Box type marine approved pressure transmitter type EMP 2 danfoss } else { Box type marine approved pressure transmitter type EMP 2 danfoss }
    EMP 2, box-type marine approved pressure transmitter

    The high accuracy pressure transmitter EMP 2 is designed for monitoring and control in marine and industrial applications and offers a reliable pressure measurement, even under harsh environmental conditions. The flexible pressure transmitter program covers absolute or gauge (relative) versions with zero and span adjustment with a 4 – 20 mA output signal.

Go to product store