Danfoss and Danish hospital lead the way in decarbonizing healthcare

Friday, June 28, 2024
  • Danish hospital Sygehus Sønderjylland’s innovative energy solution, powered by Danfoss technology and collaboration, sets a new standard for sustainable healthcare practices.
  • Two new energy-efficient heat pumps and an updated hydronic system are expected to lead to energy savings of 18,300 MWh and accelerate the hospital’s decarbonization efforts.

Sygehus Sønderjylland – the local hospital in Sønderborg located in Southern Denmark – is leading the way in ensuring a greener and more sustainable future in healthcare as they are replacing gas-based heating and cooling systems with energy-efficient technology.

Today, marked the inauguration of two new heat pumps and an updated hydronic system, which will support the hospital in their transition to become carbon neutral as they phase out fossil fuels. With a combined capacity of 2.6 MW, two Energy Machines™ heat pumps will provide the hospital with sustainable heating and cooling. Each machine is equipped with four Danfoss oil-free Turbocor® compressors. These compressors boast exceptional efficiency, particularly for cooling applications, making them an excellent fit for buildings with a high cooling demand such as hospitals, manufacturing facilities, and data centers.

Bo Libergren, Regional Councilman, says:

“We are thrilled to officially inaugurate our two new heat pumps as part of the hospital’s new customer demonstration room. This is a significant move away from fossil fuels and outdated gas boilers. At Sygehus Sønderjylland and in our region, we are committed to reducing our carbon footprint, and our aim is that this project will inspire the healthcare sector to follow our example to accelerate the green transition”.

The new solution not only reduces the hospital’s environmental impact by lowering its carbon footprint, but it also creates a more comfortable indoor climate, while setting an example of how the energy systems of the future are electrified, hydronic, and integrated.

Energy Efficiency through Integrated Systems and Sector Coupling

The two new heat pumps will replace gas and oil-based heating and cooling systems through energy-efficient technology and are expected to reduce the hospital’s annual energy consumption by around 12,500 MWh.

In addition to producing direct cooling for the hospital’s technical installations, scanners, ambulatory clinics, and wards, the hospital will use the excess heat recovered from cooling to meet the hospital process and comfort heat loads while utilizing heat to keep staff and patients comfortable. The new integrated system will also enable the hospital to become an energy provider as the hospital will provide heat to the local district heating network in terms of surplus heat to further extend the decarbonization impact to the local community. Once the system is fully implemented, the hospital expects to sell back 12,500 MWh of excess heat to the grid, which could cover the heat consumption of more than 740 average Danish households.

Jürgen Fischer, President of Danfoss Climate Solutions, says

“This partnership is a lighthouse example of how innovation and collaboration can drive sustainable change. It also showcases our commitment in Danfoss to co-develop sustainable solutions to decarbonize heating and cooling. We are proud to partner with Sygehus Sønderjylland and the district heating utility Sønderborg Varme as we set a new standard for decarbonizing the healthcare sector”.

The project has been headed by a steering committee with representatives from the Sønderborg Municipality, Sønderborg Varme A/S, Rambøll, and representatives from the hospitals in the region, and Danfoss.

For further information please contact:

Jonna Senger
Email: senger@danfoss.com 

Related applications