New whitepaper from Danfoss lays out new roadmap for decarbonizing cities.
Implementation of existing technology for buildings, transport, and sector integration can bridge half the gap in the urban GHG emissions reductions needed for a 1.5°C pathway.
Cities account for 70 % of global carbon emissions. Ultimately, the battle against climate change will be won – or lost – in cities.
Action is needed urgently to make the changes necessary to enable large-scale decarbonization. To address this challenge directly, Danfoss is today releasing a new whitepaper which sets out a clear, achievable pathway forward to enabling a green transition on a large scale. The paper shows how existing energy efficiency and electrification measures across sectors can immediately reduce emissions and accelerate a green transition in cities.
Commenting on the launch of the whitepaper, Kim Fausing, President and CEO, Danfoss, said:
As the world’s population continues its surge towards 10 billion people by 2050, it is now expected that almost 70% of the world’s inhabitants will be city dwellers by this date. In their current form, with energy demand continuing to grow, cities would produce a wholly unsustainable level of emissions that would be completely incompatible with key climate targets, such as the 1.5°C target set out by the 2015 Paris Agreement.
The whitepaper, ‘Roadmap for decarbonizing cities’, draws upon a diverse range of verified sources, including the latest data from the International Energy Agency (IEA), to demonstrate why action is needed. The whitepaper also shows how that action can be taken, and highlights how the solutions that will enable this are already available.
Key takeaways:
- Energy efficiency in cities is essential for global decarbonization. If all urban areas and cities in Europe, the US, and China invested in energy-efficient heating and cooling of buildings, this would contribute 20% to the 1.5°C target of the Paris Agreement.
- Electrification of vehicles will play a large role. Electrification of urban transport, both private (light) and public (heavy), is crucial for successful climate targets. 28% of the decarbonization necessary to stay within the 1.5°C target of the Paris Agreement would be achieved if all urban areas in Europe, the US, and China electrified private and public transport.
- Improved efficiency can accelerate the electrification of transport. Both in passenger cars, heavy duty vehicles, and in marine transport, efficiency measures can reduce the size of the batteries needed thus limiting the raw material requirements. Increasing efficiency can also bring down the demand for charging infrastructure and increase the productivity and range of the vehicle.
- Implementation of existing technology for buildings, transport, and sector integration can bridge half the gap in the urban GHG emissions reductions needed for a 1.5°C pathway.
The whitepaper analysis provides a concrete roadmap for mayors, local decisionmakers, and urban planners on how to eliminate all major drivers of the carbon footprint of cities. The paper also explores how available technologies can improve the livelihoods of citizens while at the same time making our economies more resilient and creating jobs. Ultimately, it offers a holistic and concrete view of the major opportunities for decarbonizing cities.
For further information please contact:
Amanda Chick, Global PR Lead
Ph: +357 9514 5470
Email: amanda.chick@danfoss.com