• My Apps
    My Apps You will have the option to use My apps once you login.

A simple step towards big home energy savings

Monday, February 26, 2018
Thermostatic radiator valve

A new report shows that for about 70 million European households, energy costs could be reduced significantly by upgrading heating systems with basic thermostatic radiator valves.

Heating accounts for between 48 and 69 percent of the total home energy use in 24 of the 28 EU countries. According to new evidence from the European Building Automation Controls Association (EUBAC), energy use could be reduced significantly if homeowners would replace uncontrolled, manual radiator valves with thermostatic radiator valves that automatically adjust the heating to the pre-set level. The eu.bac study estimates that about 500 million uncontrolled valves are still mounted on radiators in homes across the EU, wasting energy and money year after year.

“When a radiator uses an uncontrolled valve, it runs non-stop, even when the room has become warm. A thermostatic radiator valve can be set to heat a room to the required setting efficiently and without compromising comfort. Once the room temperature reaches that setting, the valve turns the radiator off. When the room temperature drops again, the thermostatic valve turns the radiator back on again. It is a technology that has proven its worth for decades,” explains Anders Barkholt, Vice President, Residential Heating, Danfoss.

This kind of thermostatic radiator control means homes stay warm without wasting energy e.g. when the windows have to be opened to let out excess heat. In this way, homeowners can save money while increasing comfort at all times.

Substantial energy savings potential
Thermostatic radiator valves also hold an enormous energy saving potential for society as a whole.

EUBAC has prepared a detailed country-by-country analysis based on data from the European Environment Agency on energy use and heating costs in EU homes. The study concludes that EU citizens would save a staggering €12 billion annually and reduce CO2 emissions by about 24 million tonnes if all of the 500 million radiators with uncontrolled valves in the EU were upgraded with thermostatic radiator valves. The estimate is based on an average energy saving of 18 % when installing a thermostatic radiator valve, a conservative figure that can turn out to be significantly higher.

“When it comes to home energy savings, the performance of the heating system matters a lot. Using thermostatic radiator valves is an inexpensive, no-regret solution to achieve comfortable and healthy homes at minimum costs. Since the purchase price of the thermostatic radiator valve is similar to uncontrolled valves, it seems obvious that every radiator should have a thermostatic radiator valve,” says Stephan Kolb, Head of Industry Affairs, Heating at Danfoss.

Considering the full installation cost, including work, the eu.bac study shows that the average payback time on thermostatic radiator valves is just two years. The payback time compared to the typical lifetime of a high quality thermostatic radiator valve, e.g. a Danfoss valve with a lifetime of minimum 20 years, demonstrates that the potential savings once installed are huge.

“The energy savings with thermostatic radiator valves is good for homeowners’ wallets and for national economies and ultimately for the fight against climate change,” says Anders Barkholt.


Highlights from the EUBAC report

  • About 40% of EU homes with radiator heating are equipped with uncontrolled manual valves.
  • EU citizens would save nearly €12 billion per year on their energy bills if they installed thermostatic radiator valves.
  • EU homes could save 130 TWh of energy per year.
  • EU CO2 emissions would be reduced by about 24 million tonnes.
  • The cost of these upgrades would be paid back in energy savings in just 2 years.
  • Replacement of installed thermostatic radiator valves older than 20 years could deliver additional 30 TWh savings.


For more information:
Stephan Kolb, Head of Industry Affairs, Heating, Danfoss
E-mail: stephan.kolb@danfoss.com
Phone: +32494458880

 

Zurich tower

Engineering the world of Tomorrow

Danfoss engineers advanced technologies that enable us to build a better, smarter and more efficient tomorrow. In the world’s growing cities, we ensure the supply of fresh food and optimal comfort in our homes and offices, while meeting the need for energy efficient infrastructure, connected systems and integrated renewable energy.

Our solutions are used in areas such as refrigeration, air conditioning, heating, motor control and mobile machinery.

Our innovative engineering dates back to 1933 and today Danfoss holds market-leading positions, employing more than 26,000 and serving customers in more than 100 countries. We are privately held by the founding family.