Join Danfoss at 2025 Membrane Technology Conference & Exposition

  • Overview
  • Related products
Date: 24 - 27 February, 2025
Location: Long Beach, California, USA

Danfoss highlights energy-efficient zero liquid discharge (ZLD) and seawater reverse osmosis solutions at this year’s Membrane Technology Conference

The UN Environment Programme (UNEP) estimates that 1.8 billion people will likely face absolute water scarcity, and that two-thirds of the global population will experience water stress – not at some distant point the future, but in 2025. These estimates alone illustrate the importance of finding ways to recycle and reuse more water. Yet, seawater reverse osmosis (SWRO) and zero liquid discharge (ZLD) – two of the main processes for producing more fresh water – require significant amounts of energy, at a time when the world’s focus is on decarbonizing energy-intensive industrial processes. Thankfully, it is possible to create more water while using less energy, with solutions that are readily available today.

At the 2025 Membrane Technology Conference, Danfoss experts will showcase solutions that improve energy efficiency in desalination, zero liquid discharge and brine mining processes, including:

  • High-pressure APP pumps optimized for land-based, off-shore and marine SWRO, as well as zero liquid discharge (ZLD) and minimum liquid discharge (MLD) applications. The Danfoss booth will also feature the award-winning ceramic APP pump, recipient of the Water Technology Idol at the 2024 Global Water Summit, and the Miriam Balaban Award at Euromed 2024.
  • iSave® energy recovery devices for high-pressure membrane applications. The iSave features an innovative 3-in-1 design that integrates a pressure exchanger, booster pump and motor. It recovers 94% of the high-pressure energy that would otherwise be wasted during the process, resulting in up to 60% energy savings for plant operators.
Georg Herborg

Meeting the dual challenges of water scarcity and climate change requires that we develop energy-efficient membrane processes. The less energy we use, the lower their financial costs and carbon footprint, and the more widespread these water treatments will become. This will help us meet people’s need for fresh water, while meeting the planet’s need for fewer carbon emissions.

Georg Herborg, Head of Innovation, Danfoss High Pressure Pumps

Visit us at Booth 337

Membrane Technology Conference

Long Beach Convention Center

February 24-27, 2025

Read more about the event:

Related products

  • if (isSmallPicture) { High-pressure pumps for ZLD reverse osmosis applications; } else if (isBigColumns) { High-pressure pumps for ZLD reverse osmosis applications } else { High-pressure pumps for ZLD reverse osmosis applications }
    High-pressure pumps for ZLD and MLD reverse osmosis applications

    The APP W HC pump is suitable for ZLD and MLD reverse osmosis applications used in industrial wastewater treatment.

  • if (isSmallPicture) { APP high-pressure pumps - Danfoss; } else if (isBigColumns) { APP high-pressure pumps - Danfoss } else { APP high-pressure pumps - Danfoss }
    High-pressure pumps for SWRO applications

    The range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.

  • if (isSmallPicture) { MPE 70 energy recovery device; } else if (isBigColumns) { MPE 70 energy recovery device } else { MPE 70 energy recovery device }
    Energy recovery device for medium to large SWRO applications

    The first active ERD for medium and large plants integrates highly effective isobaric pressure exchangers with a low-voltage motor to eliminate the risk of rotor overspin, reduce mixing and biofouling, and facilitate smarter automation. Covering train sizes from 1,500 m3/day and above.

     

  • if (isSmallPicture) { iSave energy recovery device - Danfoss; } else if (isBigColumns) { iSave energy recovery device - Danfoss } else { iSave energy recovery device - Danfoss }
    iSave® energy recovery devices for high-pressure membrane applications

    With a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day