Danfoss is at LIGNA to showcase the advantages of using high-pressure water mist within the sawmill industry.
Without water mist, lumber drying can be inconsistent and slow, unhealthy dust levels can harm employee safety, and non-lubricated sawmill blades can result in downtime.
Our popular NWC power pack uses water mist to solve these problems, all while optimizing productivity and minimizing waste in sawmill processes.
We will be demonstrating the Danfoss power pack, as well as our high-quality valves and nozzles, which can be incorporated into existing systems.
Improving operations delivers more than cost savings and efficiency; it also means less waste for the environment.
Discover what it's like to get faster drying, consistent quality, and less downtime.
Stop by to see our powerpack demo, running twice per day. Danfoss experts will also be on hand to discuss how you can lower costs and improve operations with our NWC power pack and high-quality components.
Visit us at Hall 025, Stand E02
LIGNA 2023
May 15-19, 2023