Innovating Better Solutions for Clean Water
We believe in a better, cleaner future for water. At Danfoss, we help businesses tackle everyday wastewater and desalination challenges through innovation and an unwavering commitment to our customers and to the planet.
This year at Aquatech Amsterdam 2023, we will display our range of energy-efficient solutions for desalination and wastewater reuse (ZLD and MLD). This includes our APP high-pressure pumps and iSave energy recovery devices as well as compatible pressure transmitters and temperature sensors for the water-pump market. At the same time, we will showcase our new MPE 70 energy recovery device designed for larger SWRO plants.
You can also get a first look at our latest pump for wastewater reuse (ZLD and MLD), which is made with ceramic parts.
Join Aquatech to consult with our team of experts and find out how to address your unique clean-water challenges. Together, we can create a future where water scarcity is no longer a privilege.
Remember to use #Aquatech23 when sharing your experience on social media. We look forward to seeing you there!
Join us from 6-9 November 2023 at our booth hall 01, booth 01.334.
Danfoss will do three presentations during the show:
“Refurbishment of products” by Kent Mentz, Sales Manager
At the Circular Economy Pavilion (hall 7, booth 07.400), Monday 6 Nov 11.30 to 12.15 and Wednesday 8 Nov 12.45 to 13.30.
“Maximizing SWRO’s energy efficiency” by Jesper Bentzen, Sales Director.
At the Circular Economy Pavilion (hall 7, booth 07.400), Tuesday 7 Nov 11.30 to 12.15 and Thursday 9 Nov 11.00 to 11.45.
“Improving energy efficiency and operational control of membrane systems: Concept of using a generator with drive (VFD)”by Daniel Schmitz, Sales Manager
At the Waste & Water Resources World Pavilion (hall 7, booth 07.508), Wednesday 8 Nov 14.35 to 14.50
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Sensors with built-in transmitter, MBT 3560, MBT 5550 & MBT 5560The MBT 3560, MBT 5550, and MBT 5560 temperature transmitter converts the input signal from a resistance sensor into a standardized output signal (e.g. Volt or mA) resulting in a compact temperature sensor with a built-in transmitter
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }MBS 9200 milibar pressure transmitter for general purpose applicationsMBS 9200 is designed for use in general purpose applications where low pressure are measured in the milibar range.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }DST P40I titanium pressure transmitter for use in corrosive environments and with aggressive mediaFor use in corrosive environments and with aggressive media, Danfoss offers the robust DST P40I pressure transmitter made of Titanium and with ceramic pressure sensing element. DST P40I is optimized for use in applications such as desalination systems, seawater cooling, and chemical processing.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Flexible temperature sensor, MBT 3270The flexible temperature sensor MBT 3270 can be used in many industrial and cooling applications such as: air compressors, hydraulics as well as cooling systems. In other words, applications where robustness, size, and performance matters.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }MBS 3000 general purpose pressure transmittersMBS 3000 is designed for use in almost all industrial applications, and offers a reliable pressure measurement, even under harsh environmental conditions.
The flexible pressure transmitter programme covers all standard output signals.